8. Additional Tools

8.1. ESI-Manager

ESI-Manager can be found through the main menu File -> ESI-Manager.

This dialog helps the user to administrate his ESI files. Here, he can add/delete/export ESI files.
_images/esi-manager.png

8.2. Network Mismatch Analyzer

If you have a network mismatch in your EtherCAT network it is not so easy to find the problem. For this you have the Network Mismatch Analyzer. If you see here some “red” entries, means that this is the start point of your network mismatch:
_images/network-mismatch.png

8.3. Line Crossed Analyzer

If you have connected a line to a wrong port, you can see in the Line Crossed Analyzer which slave is incorrectly connected. The wron entries will be red:
_images/line-crossed.png

8.4. EoE Endpoint Configuration

If you want to use EoE slaves with your local master, you can activate the EoE Endpoint.

Note

This feature is only available if the package “Tap-Windows” from OpenVPN is installed.

If this package is installed, you will see the following dialog:
_images/eoe.png
Settings
Use EoE Endpoint:

Activate EoE Endpoint support for the selected device

Network Adapter:

List of installed network adapters (TAP)

IP Address:

IP Address of the selected network adapter

8.5. Capture File

A capture file could be helpful, if you have a very large system or system is not always available. In that case you can connect to your system, save one or more snapshots into a capture file and analyse the created capture file later.

Another use case is, that your system from time to time some problems. In that case you can activate the automatic mode and create the snapshots every specific interval or based on specific master notifications.

At the moment there are the following options:
_images/capture_3.png

Filename

Base file name:

Base file name of the generated capture file name

Date:

Activate, to add the date to the generated capture file name

Time:

Activate, to add the time to the generated capture file name

Content
Process data:

Activate to add process data to the capture file (read-only)

EEPROM size:

Enter size of the EEPROM (0x86 = default, 0 = no EEPROM)

ESC Register size:

Enter size of the ESC Registers (0x400 = default, 0 = no ESC register)

CoE OD of slaves:
Select the slaves of which the CoE OD information will be captured
None:

CoE OD will be not captured

All:

CoE OD will be captured of all slaves

User defined:

CoE OD will be captured of the defined slaves by physical address (e.g. 1001-1003; 1005)

CoE OD objects:

Enter index of specific objects or all objects will be collected (e.g. 0x1018; 0x7000-0x7FFF)

SDO Info Service:

Activate to use the SDO Info Service for loading the CoE Object Dictionary instead of readying the information from the ESI file.

Automatic Mode
Interval (min):

Time to wait until next snapshot will be taken

Maximum Snapshots:

Enter count of maximum snapshots

Notifications:
Select the notifications, which will trigger a snapshot. The following notifications are availabe (for more information about notifications please refer the manual of EC-Master):
  • STATECHANGED

  • ETH_LINK_CONNECTED

  • ETH_LINK_NOT_CONNECTED

  • SLAVE_STATECHANGED

  • SLAVE_PRESENCE

  • SLAVE_INITCMD_RESPONSE_ERROR

  • STATUS_SLAVE_ERROR

  • SLAVE_UNEXPECTED_STATE

  • DC_SLV_SYNC

  • DCM_SYNC

  • FRAME_RESPONSE_ERROR

  • CYCCMD_WKC_ERROR

8.6. Project Templates

If you have a lot of slaves with the same configuration (e.g. PDOs, InitCmds) you can use a project template. In that case new slaves will be first copied from this template (if available) and then taken from the ESI cache. This behaviour is also used for the bus scan.

At the moment there are the following options:
_images/template.png

Path: Path to the selected project template

Settings
Activate:

True, for activating this project template (necessary if you want to turn it temporary off)

Ignore Revision:

The revision will be not used as search criteriom

Normally the first match will be taken from project template. If this is wrong, you can open the context menu Select from Project Template and select another one:
_images/template_3.png