7. Command Line Interface
For helping users in some special situations and to do not confuse other users the EC-Lyser supports a small command line interface:
- /REMOTE=”127.0.0.1:6000:0:0”:
- Runs diagnosis with a remote system, where IP address is “127.0.0.1”, port is 6000, MainDevice instance is set to 0 and protocol is set to RAS. It is also supported to use the DNS name instead of the IP address
- /LOCAL=”127.0.0.1”:
- Runs diagnosis with the local system and the network adapter with IP address “127.0.01” will be chosen