5.7. Xilinx EMAC - emllEMAC

The parameters to the EMAC Ethernet MAC Link Layer are setup-specific. The function “CreateLinkParmsFromCmdLineEMAC” in EcSelectLinkLayer.cpp demonstrates how to initialize the Link Layer instance.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_EMAC

Physical base address of register block (4k)

PHY address

Receive interrupt number (IRQ)

Physical length of register block

EC_TRUE: copy buffer before processing, EC_FALSE: Use buffers from DMA (default)