# Technical overview ## Support SubDevices and topologies EC-Master supports all currently existing SubDevice types and possible topologies: - SubDevices with 32 bit or 64 bit system time register (0x0910) - Reference Clock with 32 bit or 64 bit system time register (0x0910) - Reference Clock as first SubDevice (auto increment address 0) or in the middle. Only SubDevices behind the reference clock could be synchronized. - Drift compensation with 32 bit or 64 bit ARMW command in the cyclic frame - Topologies: Line, Daisy chain, Daisy chain with drop lines, tree structure, star topology with EK1122 junctions ![EtherCAT network topology diagrams showing line, daisy chain, tree structure, and star topologies supported for Distributed Clocks with a DC Reference Clock and the SubDevices following it.](../Media/DC_Topologie.png) ## Typical Bus Timing The following diagram gives detailed information about the timing of the system: ![Timing diagram showing the relationship between the MainDevice Job Task cycle, EtherCAT frame send time, SYNC signals, propagation delay for Distributed Clocks and the data flow of Input and Output values.](../Media/Typical_Bus_Timing.png) The timing of the Job Task must be accurate if the system must operate in real-time. It can be disturbed by jitter or drift. Small jitter values are irrelevant, but high jitter values can compromise process data exchange by causing delays that violate strict cycle deadlines. Timing disturbances may have various causes on the MainDevice system like hardware or software delays which are beyond the EC-Master stack’s control. However, different DCM modes and parameters are available to compensate the natural drift of MainDevice and SubDevices and to fine-tune synchronization. ## Implementation Details The generation of Sync impulses is started after initialization and sending of 10000 FRMW frames which are required to bring SubDevices initially into sync. After this FRMW generation a grace period of 50 ms under real-time OSes is used and 500 ms using Windows is configured before the start of cyclic operations of SubDevices, which causes the Sync impulse generation to be delayed by this grace period. Initial propagation delay measurement and offset compensation commands are not part of the ENI file. The ARMW command for drift compensation is part of the cyclic frame. ## SubDevices in sync SubDevices in sync means that the system time difference of all DC SubDevices does not exceed a configured limit. Out of sync is detected individually and immediately for each SubDevice. The MainDevice awaits that the SubDevices are in sync in MainDevice state transition INIT->PREOP. Therefore the MainDevice state transition may timeout if the SubDevices do not get in sync. Due to technology the SubDevices are always getting in sync as long as there is no error in setup. In order to detect system time difference exceeding, [Sync Window Monitoring](#sync-window-monitoring) is used. ## Sync Window Monitoring Sync Window Monitoring must be explicitly enabled in the configuration. The system time difference exceeding detection in Sync Window Monitoring uses a deviation limit and a settle time and is issued continuously with configured commands (Ado 0x092C) in cyclic frames. In sync is assumed if there is no violation of the system time difference limit (for all DC SubDevices!) detected within the settle time. The deviation limit (dwDevLimit) and settle time (dwSettleTime) can be configured using [`emDcConfigure()`](dc_api.html.md#_CPPv413emDcConfigure10EC_T_DWORDPK17EC_T_DC_CONFIGURE). If the configuration only contains the cyclic commands for SAFE-OP or OP (e.g. ET9000) the MainDevice queues acyclic datagrams (Ado 0x092C) for system time difference measurement. If there are less than two DC SubDevices on the bus (e.g. if the reference clock is the only DC SubDevices on bus), Sync Window Monitoring is skipped. If it is skipped, because it is not enabled in configuration or there are less than two DC SubDevices on bus, SubDevices are immediately considered in sync.