/** ---------------------------------------------------------------------------
 * \file        EcDemoParms.h
 * \brief       Application specific settings for EC demo
 * \author      Holger Oelhaf
 * \copyright   acontis technologies GmbH, Weingarten, Germany
 *---------------------------------------------------------------------------*/

#ifndef INC_ECDEMOPARMS_H
#define INC_ECDEMOPARMS_H 1

/*-DEFINES-------------------------------------------------------------------*/
#if (!defined INCLUDE_EC_LOGGING) && (!defined EXCLUDE_EC_LOGGING)
#define INCLUDE_EC_LOGGING
#endif

/*-INCLUDES------------------------------------------------------------------*/
#include <ctype.h>

/*-FORWARD DECLARATIONS------------------------------------------------------*/
struct _EC_T_FMU;

/*-DEFINES-------------------------------------------------------------------*/
#define DEFAULT_BUS_CYCLE_TIME_NSEC      1000000
#define DEFAULT_DEMO_DURATION             600000

#if (defined EC_DEMO_TINY)
#ifndef MASTER_CFG_ECAT_MAX_BUS_SLAVES
#define MASTER_CFG_ECAT_MAX_BUS_SLAVES         8    /* max number of pre-allocated bus slave objects */
#endif
#define MASTER_CFG_MAX_ACYC_FRAMES_QUEUED      6    /* max number of acyc frames queued, 127 = the absolute maximum number */
#define MASTER_CFG_MAX_ACYC_BYTES_PER_CYC    512    /* max number of bytes sent during eUsrJob_SendAcycFrames within one cycle */
#else
#ifndef MASTER_CFG_ECAT_MAX_BUS_SLAVES
#define MASTER_CFG_ECAT_MAX_BUS_SLAVES       256    /* max number of pre-allocated bus slave objects */
#endif
#define MASTER_CFG_MAX_ACYC_FRAMES_QUEUED     32    /* max number of acyc frames queued, 127 = the absolute maximum number */
#define MASTER_CFG_MAX_ACYC_BYTES_PER_CYC   4096    /* max number of bytes sent during eUsrJob_SendAcycFrames within one cycle */
#endif /* EC_DEMO_TINY */

#define MASTER_CFG_MAX_ACYC_CMD_RETRIES        3

#define ETHERCAT_STATE_CHANGE_TIMEOUT      15000    /* master state change timeout in ms */
#define ETHERCAT_SCANBUS_TIMEOUT           10000    /* scanbus timeout in ms, see also EC_SB_DEFAULTTIMEOUT */

#if (defined EC_DEMO_TINY)
#define COMMAND_LINE_BUFFER_LENGTH 128
#define MAX_LINKLAYER   2
#else
#define COMMAND_LINE_BUFFER_LENGTH 512
#define MAX_LINKLAYER   5
#endif

#define DEMO_MAX_NUM_OF_AXIS                   6    /* max number of axis that can be used in DS402 demos */
#define DEMO_MAX_NUM_OF_CAM_TABLES             1    /* max number of CAM tables */

/* Motion */
#define DEMO_CFG_DEFAULT_FILENAME                       "DemoConfig.xml"

/*-TYPEDEFS------------------------------------------------------------------*/

/********************************************************************************/
/** \brief The policy to become ACTIVE determines under which circumstances the Master may switch to ACTIVE.
 * Depending on the policy in effect, the INACTIVE Master may evaluate whether network operation by another ACTIVE Master is currently or was previously detected.
 * This specific redundancy logic must be managed at the application level.
 */
typedef enum _T_eBecomeActivePolicy
{
    eBecomeActivePolicy_Unknown = 0,    /**< Unknown policy */
    eBecomeActivePolicy_Autonomous = 1, /**< Become ACTIVE if network not operated by another Master */
    eBecomeActivePolicy_Gated = 2,      /**< Become ACTIVE after network operation by another Master was detected, and other Master network operation stopped */
    eBecomeActivePolicy_Forced = 3,     /**< Become ACTIVE immediately */
    eBecomeActivePolicy_Suspended = 4,  /**< Never become ACTIVE */

    /* Borland C++ datatype alignment correction */
    eBecomeActivePolicy_BCppDummy = 0xFFFFFFFF
} T_eBecomeActivePolicy;

/* demo application parameters */
typedef struct _T_EC_DEMO_APP_PARMS
{
    EC_T_OS_PARMS       Os;                             /* operating system parameters */
    EC_T_DWORD          dwCpuIndex;                     /* CPU index */
    EC_T_CPUSET         CpuSet;                         /* CPU-set for SMP systems */
    EC_T_DWORD          dwJobsThreadPrio;               /* JobTask priority (default: JOBS_THREAD_PRIO) */
    EC_T_DWORD          dwJobsThreadStackSize;          /* JobTask stack size (default: JOBS_THREAD_STACKSIZE) */

    /* link layer */
    EC_T_LINK_PARMS*    apLinkParms[MAX_LINKLAYER];     /* link layer parameters array */
    EC_T_DWORD          dwNumLinkLayer;                 /* link layer count in apLinkParms */

    /* configuration */
    EC_T_CNF_TYPE       eCnfType;                       /* configuration data type */
    EC_T_BYTE*          pbyCnfData;                     /* configuration data filename / buffer */
    EC_T_DWORD          dwCnfDataLen;                   /* configuration data length in bytes */
    EC_T_CHAR           szENIFilename[256];             /* ENI filename string */
    EC_T_CHAR           szLicenseKey[64];               /* license key string */
    EC_T_UINT64         qwOemKey;                       /* OEM key */
    EC_T_DWORD          dwMaxBusSlaves;                 /* max number of slaves (MASTER_CFG_ECAT_MAX_BUS_SLAVES) */

    /* timing */
    EC_T_DWORD          dwBusCycleTimeNsec;             /* bus cycle time [ns] */
    EC_T_DWORD          dwDemoDuration;                 /* demo duration [ms] */

    /* logging */
    EC_T_INT            nVerbose;                       /* verbosity level */
    EC_T_DWORD          dwAppLogLevel;                  /* demo application log level (derived from verbosity level) */
    EC_T_DWORD          dwMasterLogLevel;               /* Master / Monitor / Simulator stack log level (derived from verbosity level) */
    EC_T_CHAR           szLogFileprefix[64];            /* log file prefix string */
    EC_T_DWORD          dwLogBufferMaxMsgCnt;           /* max number of buffered messages (DEFAULT_LOG_MSG_BUFFER_SIZE)  */
    EC_T_BOOL           bPcapRecorder;                  /* EtherCAT packet capture in pcap format (wireshark) enabled */
    EC_T_CHAR           szPcapRecorderFileprefix[64];   /* log file prefix string */
    EC_T_DWORD          dwPcapRecorderBufferFrameCnt;   /* max number of buffered frames */

    /* RAS */
    EC_T_BOOL           bStartRasServer;
    EC_T_BYTE           abyRasServerIpAddress[4];       /* Remote Access Server (RAS) listen IP address */
    EC_T_WORD           wRasServerPort;                 /* Remote Access Server (RAS) listen port */
    EC_T_BYTE           abyRasClientIpAddress[4];       /* Remote Access Server (RAS) connect IP address */
    EC_T_WORD           wRasClientPort;                 /* Remote Access Server (RAS) connect port */
    EC_T_BOOL           bRasAccessControlEnabled;       /* Remote Access Server (RAS) access control enabled */
    EC_T_DWORD          dwRasAccessLevel;               /* Remote Access Server (RAS) access control level */

    /* mailbox gateway server */
    EC_T_WORD           wMbxGatewayServerPort;          /* Mailbox Gateway server port */

    /* DCM */
    EC_T_BOOL           bDcmConfigure;                  /* DCM configuration enabled */
    EC_T_DCM_MODE       eDcmMode;                       /* DCM mode */
    EC_T_BOOL           bDcmSyncToCycleStart;           /* DCM sync to cycle start */
    EC_T_BOOL           bDcmControlLoopDisabled;        /* DCM control loop disabled */
    EC_T_BOOL           bDcmLogEnabled;                 /* DCM logging enabled */
    EC_T_INT            nCtlSetValNsec;                 /* DCM distance between cyclic frame send time and DC base on bus */

    /* master redundancy */
    T_eBecomeActivePolicy eBecomeActivePolicy;          /* Master redundancy policy to become active */
    EC_T_BOOL           bMasterRedSwitchTopology;       /* Master redundancy switch topology */

    /* additional parameters for the different demos. TODO: reword */
    EC_T_DWORD          dwMasterInstanceId;             /* Master instance id */
    EC_T_DWORD          dwPerfMeasLevel;                /* performance measurement level */
    EC_T_BOOL           bPerfMeasShowCyclic;            /* show performance values cyclically  */
    EC_T_WORD           bFlash;                         /* flashing process data (Master: OUTPUTs / Simulator: INPUTs) */
    EC_T_WORD           wFlashSlaveAddr;                /* flashing process data (Master: OUTPUTs / Simulator: INPUTs) slave station address */

    struct {
        EC_T_DWORD dwOffset;                            /* process data bit offset */
        EC_T_DWORD dwSize;                              /* process data bit size */
        EC_T_DWORD dwValue;                             /* process data to set */
        EC_T_DWORD dwDuration;                          /* duration of how long process data should be set [ms]. 0 == forever */
    }                   SetProcessDataBits;             /* process data access helper struct */
    EC_T_DWORD          dwNotifyCode;                   /* notification code for ecatNotifyApp */
    EC_T_NOTIFYPARMS    NotifyParms;                    /* notification parameter for ecatNotifyApp */

    /* EC-Daq */
    EC_T_BOOL           bDaqRecorder;                   /* DAQ recorder config file enabled */
    EC_T_CHAR           szDaqRecorder[256];             /* DAQ recorder config filename string */

    /* EC-Simulator */
    EC_T_DWORD          dwSimulatorInstanceId;          /* simulator instance id */
    EC_T_BOOL           bDisableProcessDataImage;       /* don't allocate Process Data Image at EC-Simulator (Master ENI / Simulator ENI mismatch support) */
    EC_T_BOOL           bConnectHcGroups;               /* auto-connect floating Hot Connect groups / disconnect all Hot Connect groups */
    EC_T_DWORD          dwCfgDeviceConnectionCount;
    EC_T_SIMULATOR_DEVICE_CONNECTION_DESC aoDeviceConnection[MAX_LINKLAYER]; /* see EC_SIMULATOR_DEVICE_CONNECTION_TYPE_... */

    /* DS402 */
    EC_T_DWORD          dwDS402NumSlaves;               /* DS402 simulated slaves count */
    EC_T_WORD           awDS402SlaveAddr[DEMO_MAX_NUM_OF_AXIS]; /* station fixed adresses of DS402 simulated slaves */

    /* EC-FMU */
    EC_T_CHAR           szFmuLogfile[256];               /* FMU log file */
    EC_T_CHAR           szFmuFilename[256];              /* FMU file to be loaded */
    EC_T_CHAR           szCsvMappingFilename[256];       /* FMU variables to PDO variables mapping (CSV) */

    /* EAP */
    EC_T_BYTE           abyIpAddress[4];                /* IP address */

    /* EC-Monitor */
    EC_T_BOOL           bPcapProcessing;                /* packet capture file processing enabled */
    EC_T_CHAR           szPcapFilename[256];            /* packet capture file name */
    EC_T_CHAR           szEBIFilename[256];             /* EBI export filename string */

    /* Motion */
    EC_T_CHAR           szCfgFilePath[256];
    EC_T_BOOL           bCmdMode;                       /* Command Mode: Get commands from EC-STA */

    /* MQTT */
    EC_T_CHAR           szMqttServerUri[256];
    EC_T_DWORD          dwMqttChgUpdateTime;            /* MQTT publish change detection minimum time */
    EC_T_DWORD          dwMqttCycUpdateTime;            /* MQTT publish cyclic time */

    /* read CoE object dictionary from device */
    EC_T_BOOL           bReadOD;
    EC_T_WORD           wReadODSlaveAddr;

    /* print process variable name and offset for all variables of all slaves */
    EC_T_BOOL           bPrintVars;

    /* EoE */
    EC_T_CHAR szEoeTap[32];
    EC_T_JUNCTION_REDUNDANCY_MODE eJunctionRedMode;

    /* Fingerprint */
    EC_T_BOOL bUseFingerprint;
    EC_T_BYTE byFingerprintMethod;

    /* Frame mirror */
    EC_T_LINK_PARMS* pLinkParmsMirror;                  /* Frame mirror link layer */

    /* TLS */
    EC_T_CHAR           szTlsCert[256];             /* TLS certificate filename string */
    EC_T_CHAR           szTlsPrivKey[256];          /* TLS private key filename string */
} T_EC_DEMO_APP_PARMS;

/* demo application context */
typedef struct _T_EC_DEMO_APP_CONTEXT
{
    T_EC_DEMO_APP_PARMS       AppParms;                 /* demo application parameters */
    EC_T_LOG_PARMS            LogParms;                 /* log parameters */
    EC_T_DWORD                dwInstanceId;             /* instance id */
    EC_T_VOID*                pvJobTaskEvent;           /* job task event */
    EC_T_BOOL                 bJobTaskRunning;          /* job task running flag */
    EC_T_BOOL                 bJobTaskShutdown;         /* job task shutdown request flag */
#if (defined __cplusplus)
    class CEmNotification*    pNotificationHandler;     /* notification handler */
#else
    struct _T_CEmNotification* pNotificationHandler;    /* notification handler */
#endif
    EC_T_VOID*                pvCycFrameReceivedEvent;  /* cyclic frame received event */
    EC_T_DWORD                dwPerfMeasLevel;          /* performance measurement level */
    EC_T_VOID*                pvPerfMeas;               /* performance measurement object */
    struct _T_MY_APP_DESC*    pMyAppDesc;               /* my app descriptor */
    struct _T_MASTER_RED_DEMO_PARMS* pMasterRedParms;   /* Master redundancy parameters */
    struct _T_EC_MONITOR_DEMO_PARMS* pMonitorParms;     /* EC-Monitor parameters */
    EC_T_VOID*                pTimingTaskContext;       /* Timing Task Context for various Busshift, Mastershift, MasterRefClock and DCX.Mastershift mode */
#if (defined __cplusplus)
    class CPcapRecorder*      pPcapRecorder;            /* Pcap recorder instance */
    class CFrameMirror*       pFrameMirror;             /* Frame mirror instance */
#endif

    struct _EC_T_FMU*         pFmu;
} T_EC_DEMO_APP_CONTEXT;

/*-GLOBAL VARIABLES-----------------------------------------------------------*/
extern volatile EC_T_BOOL  bRun;                        /* global demo run flag */

/*-FORWARD DECLARATIONS------------------------------------------------------*/
struct _T_EC_DEMO_APP_CONTEXT;

/*-FUNCTION DECLARATION------------------------------------------------------*/
EC_T_DWORD PrepareCommandLine(EC_T_INT nArgc, EC_T_VOID* ppArgv, EC_T_CHAR* szCommandLine);

EC_T_VOID  ResetAppParms(T_EC_DEMO_APP_CONTEXT* pAppContext, T_EC_DEMO_APP_PARMS* pAppParms);
EC_T_VOID  FreeAppParms(T_EC_DEMO_APP_CONTEXT* pAppContext, T_EC_DEMO_APP_PARMS* pAppParms);
EC_T_VOID  SetLogLevels(T_EC_DEMO_APP_PARMS* pAppParms);
#ifdef __cplusplus
EC_T_DWORD SetAppParmsFromCommandLine(struct _T_EC_DEMO_APP_CONTEXT* pAppContext, const EC_T_CHAR* szCommandLine, T_EC_DEMO_APP_PARMS* pAppParms, EC_T_CHAR** pszNextCommandLine = EC_NULL);
#else
EC_T_DWORD SetAppParmsFromCommandLine(struct _T_EC_DEMO_APP_CONTEXT* pAppContext, const EC_T_CHAR* szCommandLine, T_EC_DEMO_APP_PARMS* pAppParms, EC_T_CHAR** pszNextCommandLine);
#endif
EC_T_VOID  SetAppParmsLogging(T_EC_DEMO_APP_CONTEXT* pAppContext, T_EC_DEMO_APP_PARMS* pAppParms);

EC_T_VOID ShowSyntaxAppUsage(T_EC_DEMO_APP_CONTEXT* pAppContext);
EC_T_VOID ShowSyntaxCommon(T_EC_DEMO_APP_CONTEXT* pAppContext);
EC_T_VOID ShowSyntaxApp(T_EC_DEMO_APP_CONTEXT* pAppContext);
EC_T_VOID ShowSyntaxLinkLayer();
static EC_INLINESTART EC_T_VOID ShowSyntax(T_EC_DEMO_APP_CONTEXT* pAppContext)
{
    ShowSyntaxAppUsage(pAppContext);
    ShowSyntaxCommon(pAppContext);
    ShowSyntaxApp(pAppContext);
#if (!defined EC_RAS_CLIENT_DEMO)
    ShowSyntaxLinkLayer();
#endif
#if (EC_OS == EC_OS_XENOMAI)
    EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "For Xenomai versions older than 3.0.6 please try @@ instead of -- in the command line \n"));
    EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "This is a well-known Xenomai3 bug \n"));
#endif
} EC_INLINESTOP

/*****************************************************************************/
/**
 * \brief convert a string to an unsigned long long
 *
 * \return unsigned long long
 */
static EC_INLINESTART EC_T_UINT64 EcStrtoull(const EC_T_CHAR* szNptr, EC_T_CHAR** pszEndptr, EC_T_INT nBase)
{
    const EC_T_CHAR* szLocalString = EC_NULL;
    EC_T_INT64 nAcc = 0;
    EC_T_INT64 nCutoff = 0;
    EC_T_INT64 nCutlim = 0;
    EC_T_INT nCharacter = 0;
    EC_T_INT nNeg = 0;
    EC_T_INT nAny = 0;

    /* see strtoq for comments to logic below */
    szLocalString = szNptr;
    do
    {
        nCharacter = (EC_T_BYTE)*szLocalString++;
    }
    while (' ' == nCharacter);
    if (nCharacter == '-')
    {
        nNeg = 1;
        nCharacter = *szLocalString++;
    }
    else
    {
        nNeg = 0;
        if (nCharacter == '+')
        {
            nCharacter = *szLocalString++;
        }
    }
    if (((nBase == 0) || (nBase == 16)) && (nCharacter == '0') && ((*szLocalString == 'x') || (*szLocalString == 'X')))
    {
        nCharacter = szLocalString[1];
        szLocalString += 2;
        nBase = 16;
    }
    if (nBase == 0)
    {
        nBase = ((nCharacter == '0') ? 8 : 10);
    }
    /* BIONIC: avoid division and modulo for common cases */
#define  CASE_BASE(x) \
            case x: nCutoff = ((EC_T_UINT64)-1) / x; \
                nCutlim = ((EC_T_UINT64)-1) % x; \
            break

    switch (nBase)
    {
        CASE_BASE(8);
        CASE_BASE(10);
        CASE_BASE(16);
    default:
        nCutoff = ((EC_T_UINT64)-1) / nBase;
        nCutlim = ((EC_T_UINT64)-1) % nBase;
    }
#undef CASE_BASE

    for (nAcc = 0, nAny = 0;; nCharacter = (EC_T_BYTE)*szLocalString++)
    {
        if ((nCharacter >= '0') && (nCharacter <= '9'))
        {
            nCharacter = nCharacter - '0';
        }
        else if ((nCharacter >= 'a') && (nCharacter <= 'f'))
        {
            nCharacter = nCharacter - 'a' + 10;
        }
        else if ((nCharacter >= 'A') && (nCharacter <= 'F'))
        {
            nCharacter = nCharacter - 'A' + 10;
        }
        else
        {
            break;
        }
        if (nCharacter >= nBase)
        {
            break;
        }
        if (nAny < 0)
        {
            continue;
        }
        if ((nAcc > nCutoff) || ((nAcc == nCutoff) && (nCharacter > nCutlim)))
        {
            nAny = -1;
            nAcc = -1;
        }
        else
        {
            nAny = 1;
            nAcc *= (EC_T_UINT64)nBase;
            nAcc += nCharacter;
        }
    }
    if (nNeg && (nAny > 0))
    {
        nAcc = -nAcc;
    }
    if (pszEndptr != 0)
    {
        *pszEndptr = (EC_T_CHAR*)(nAny ? szLocalString - 1 : szNptr);
    }
    return nAcc;
} EC_INLINESTOP

static EC_INLINESTART EC_T_BOOL IsLinkLayerTimingSet(EC_T_LINK_PARMS** pLinkParms)
{
    EC_T_BOOL bIsSet = EC_FALSE;
    EC_T_WORD i = 0;
    for (i = 0; i < MAX_LINKLAYER; i++)
    {
        if ((EC_NULL != pLinkParms) && (EC_NULL != pLinkParms[i]) && (eLinkLayerTiming_Undefined != pLinkParms[i]->oLinkLayerTimingTask.eLinkLayerTiming))
        {
            bIsSet = EC_TRUE;
        }
    }
    return bIsSet;
} EC_INLINESTOP

#endif /* INC_ECDEMOPARMS_H */

/*-END OF SOURCE FILE--------------------------------------------------------*/