# Real-time Ethernet Driver (RtEth) The EC-Master currently supports a variety of different Real-time Ethernet Driver modules, each contained in a single library file, which is loaded by the core library dynamically. The EC-Master EtherCAT® MainDevice stack shipment consist of a MainDevice core library (e.g. EcMaster.dll for Windows, libEcMaster.a for Linux) and one (or more) libraries each containing support for one specific Real-time Ethernet Driver module. Which library actually is loaded depends on the Link Layer parameters at runtime. Real-time means operating directly on the network adapter’s register set instead of using the operating system’s native driver. The principle of the Real-time Ethernet Driver selection is that the Real-time Ethernet Driver name (Real-time Ethernet Driver identification) is used to determine the location and name of a registration function called by the EC-Master and registers function pointers that allow access to the Real-time Ethernet Driver functional entries. The EtherCAT® Real-time Ethernet Driver will be initialized using a Real-time Ethernet Driver specific configuration parameter set. A pointer to this parameter set is part of the initialization settings of the EC-Master when calling the function [`emInitMaster()`](api_general_functions.html.md#_CPPv412emInitMaster10EC_T_DWORDPK22EC_T_INIT_MASTER_PARMS). The EC-Master supports two Real-time Ethernet Driver operating modes. If the Real-time Ethernet Driver operates in interrupt mode all received Ethernet frames will be processed immediately in the context of the Real-time Ethernet Driver receiver task. When using the polling mode the EC-Master will call the Real-time Ethernet Driver receiver polling function prior to processing received frames. **Real-time Ethernet Driver and PHY OS Driver** Some operating systems, e.g. Linux and Xenomai, provide drivers for most common Ethernet controllers and their related physical transceivers (PHY). The manufacturer specific PHY circuits can be handled by a dedicated driver. Using the PHY OS Driver interface it is possible to use the manufacturer’s dedicated PHY driver without modification of the acontis optimized Real-time Ethernet Driver. Depending on the hardware architecture, an additional module from acontis, e.g. atemsys for Linux, grants access to the MDIO bus to the OS drivers, or request MDIO operations from the OS drivers. ![EMLL architecture diagram showing the layers from application and EC-Master stack through the link-layer abstraction interface down to OS-specific and hardware network drivers](../Media/emll_phy_os_driver_architecture.png) #### NOTE Real-time Ethernet Driver modules not listed here may be available if purchased additionally. Not all Real-time Ethernet Driver modules support interrupt mode.