# Dongled version The Master library is encrypted and requires a dongle to execute. The following dongles are supported: - USB dongle - ASIC dongle - Virtual dongle using a WibuCmRaU file ## Licensing using a virtual WibuCmRaU File on Linux To create a virtual dongle using a WibuCmRaU file on a Linux machine, the following steps are required: - Download the codemeter package from Wibu website and install it on the linux machine: - Import the LIF file provided by acontis : ```batch cmu --import --file *.WibuCmLIF ``` - List the Wibu licenses, to get the serial number : ```batch cmu --list ``` - Use the serial number to generate a WibuCmRaC file : ```batch cmu --serial your_serial_number --context 6001978 --file *.WibuCmRaC ``` - Send the WibuCmRaC to acontis and acontis will provide a WibuCmRaU file. - Import the WibuCmRaU file : ```batch cmu --import --file *.WibuCmRaU ``` ## Maintain the license after a linux image update In case of a complete Linux image update, the following steps are required: - Make a backup of the WibuCmRaU file and the following folder /var/lib/Codemeter/CmAct from the old image. - On the new image install Codemeter - Restore the 6001978_\* files from /var/lib/Codemeter/CmAct - Change the user rights of the 4 files to daemon : ```batch sudo chown daemon:daemon 6001978_* ``` - Import the WibuCmRaU backup file : ```batch cmu --import --file *.WibuCmRaU ```