# EtherCAT® Mailbox Transfer
To be able to initiate a mailbox transfer the client has to create a mailbox transfer object first. This mailbox transfer object also contains the memory where the data to be transferred is stored. The one client that initiated the mailbox transfer will be notified about a mailbox transfer completion by the `emNotify()` callback function.
To be able to identify the transfer which was completed the client has to assign a unique transfer identifier for each mailbox transfer. The mailbox transfer object can only be used for one single mailbox transfer. If multiple transfers shall be initiated in parallel the client has to create one transfer object for each. The transfer object can be re-used after mailbox transfer completion.
Typical mailbox transfer sequence:
1. Create a transfer object (for example an SDO download transfer object).
: ```cpp
MbxTferDesc.dwMaxDataLen = 10
MbxTferDesc.pbyMbxTferDescData=(EC_T_PBYTE)OsMalloc(MbxTferDesc.dwMaxDataLen)
pMbxTfer = emMbxTferCreate(&MbxTferDesc)
state of the transfer object = Idle
```
2. Copy the data to be transferred to the SubDevice into the transfer object, determine the transfer ID, store the client ID in the object and initiate the transfer (e.g. an SDO download). A transfer may only be initiated if the state of the transfer object is Idle.
: ```cpp
OsMemcpy(pMbxTfer->pbyMbxTferData, "0123456789", 10);
pMbxTfer->dwTferId = 1;
pMbxTfer->dwClntId = dwClntId;
pMbxTfer->dwDataLen=10;
dwResult = emCoeSdoDownloadReq(pMbxTfer, dwSlaveId, wObIndex, ...);
state of the transfer object = Pend or TferReqError
```
The state will then be set to Pend to indicate that this mailbox transfer object currently is in use and the transfer is not completed.
If the mailbox transfer cannot be initiated the EC-Master will set the object into the state TferReqError - in such cases the client is responsible to set the state back into Idle.
3. If the mailbox transfer is completed the notification callback function of the corresponding client ( `emNotify()`) will be called with a pointer to the mailbox transfer object. The state of the transfer object is set to TferDone prior to calling `emNotify()`.
: ```cpp
if( dwResult != EC_E_NOERROR ) { ... }
emNotify( EC_NOTIFY_MBOXRCV, pParms )
state of the transfer object = TferDone
```
4. In case of errors the appropriate error handling has to be executed. The application must set the transfer object state to Idle.
: ```cpp
if( pMbxTfer->dwErrorCode != EC_E_NOERROR ) { ... }
In emNotify: application may set transfer object state to Idle
```
5. Delete the transfer object. Alternatively this object can be used for the next transfer.
: ```cpp
emMbxTferDelete(pMbxTfer);
OsFree(MbxTferDesc.pbyMbxTferDescData);
```
## Mailbox transfer object states
The following states exist for a mailbox transfer object:
### enum EC_T_MBXTFER_STATUS
*Values:*
### enumerator eMbxTferStatus_Idle
Mailbox transfer object not in use
### enumerator eMbxTferStatus_Pend
Mailbox transfer in process
### enumerator eMbxTferStatus_TferDone
Mailbox transfer completed
### enumerator eMbxTferStatus_TferReqError
Mailbox transfer request error
### enumerator eMbxTferStatus_TferWaitingForContinue
Mailbox transfer waiting for continue, object owned by application
A mailbox transfer will be processed by the EC-Master independently from the client’s timeout setting. Some types of mailbox transfers can be cancelled by the client, e.g. if the client’s timeout elapsed.
After completion of the mailbox transfer (with timeout) the client may finally set the transfer object into the state [`EC_T_MBXTFER_STATUS::eMbxTferStatus_Idle`](#_CPPv4N19EC_T_MBXTFER_STATUS19eMbxTferStatus_IdleE).
New mailbox transfers can only be requested if the object is in the state [`EC_T_MBXTFER_STATUS::eMbxTferStatus_Idle`](#_CPPv4N19EC_T_MBXTFER_STATUS19eMbxTferStatus_IdleE).
#### SEE ALSO
[`emMbxTferAbort()`](#_CPPv414emMbxTferAbort10EC_T_DWORDP12EC_T_MBXTFER)
## emMbxTferCreate
### static [EC_T_MBXTFER](#_CPPv412EC_T_MBXTFER) \*ecatMbxTferCreate([EC_T_MBXTFER_DESC](#_CPPv417EC_T_MBXTFER_DESC) \*pMbxTferDesc)
### [EC_T_MBXTFER](#_CPPv412EC_T_MBXTFER) \*emMbxTferCreate([EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwInstanceID, [EC_T_MBXTFER_DESC](#_CPPv417EC_T_MBXTFER_DESC) \*pMbxTferDesc)
Creates a mailbox transfer object.
While a mailbox transfer is in process the related transfer object and the corresponding memory may not be accessed. After a mailbox transfer completion the object may be used for the next transfer. The mailbox transfer object has to be deleted by calling ecatMbxTferDelete if it is not needed any more.
* **Parameters:**
* **dwInstanceID** – [in] Instance ID (Multiple EtherCAT Network Support)
* **pMbxTferDesc** – [in] Pointer to the mailbox transfer descriptor. Determines details of the mailbox transfer.
* **Returns:**
* Pointer to the created mailbox transfer object if successful
* EC_NULL on error (No memory left)
### struct EC_T_MBXTFER_DESC
### Public Members
### [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwMaxDataLen
Maximum amount of data bytes that shall be transferred using this object. A mailbox transfer type without data transfer will ignore this parameter.
### [EC_T_BYTE](toc_api.html.md#_CPPv49EC_T_BYTE) \*pbyMbxTferDescData
Pointer to byte stream carrying in and out data of mailbox content
### struct EC_T_MBXTFER
### Public Members
### [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwClntId
[] Client ID
### [EC_T_MBXTFER_DESC](#_CPPv417EC_T_MBXTFER_DESC) MbxTferDesc
[out] Mailbox transfer descriptor. All elements of pMbxTferDesc will be stored here.
### [EC_T_MBXTFER_TYPE](#_CPPv417EC_T_MBXTFER_TYPE) eMbxTferType
[] This type of information is written to the Mailbox Transfer Object by the last call to a mailbox command function. It may be used as information, and is required to fan out consecutive notifications. This value is only valid until the next relevant mailbox API call, where this value may be overwritten.
### [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwDataLen
[] Amount of data bytes for the next mailbox download transfer. If the mailbox transfer does not transfer data to the slave this parameter will be ignored. This element has to be set to an appropriate value every time prior to initiating a new download request. When either a download or upload transfer is completed (emNotify) this value will contain the amount of data that was actually transferred.
### [EC_T_BYTE](toc_api.html.md#_CPPv49EC_T_BYTE) \*pbyMbxTferData
[in/out] Pointer to data. In case of a download transfer the client has to store the data in this location. In case of an upload transfer this element points to the received data. Access to data that was uploaded from a slave is only valid within the notification function because the buffer will be re-used by the master. These data have to be copied into a separate buffer in case it has to be used later by the client.
### [EC_T_MBXTFER_STATUS](#_CPPv419EC_T_MBXTFER_STATUS) eTferStatus
[out] Transfer state. After a new transfer object is created the state will be set to eMbxTferStatus_Idle.
### [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwErrorCode
[out] Error code of a mailbox transfer that was terminated with error
### [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwTferId
[] Transfer ID. For every new mailbox transfer a unique ID has to be assigned. This ID can be used after mailbox transfer completion to identify the transfer.
### [EC_T_MBX_DATA](#_CPPv413EC_T_MBX_DATA) MbxData
[] Mailbox data. This element contains mailbox transfer data, e.g. the CoE object dictionary list.
### enum EC_T_MBXTFER_TYPE
*Values:*
### enumerator eMbxTferType_COE_SDO_DOWNLOAD
CoE SDO download
### enumerator eMbxTferType_COE_SDO_UPLOAD
CoE SDO upload
### enumerator eMbxTferType_COE_GETODLIST
CoE Get object dictionary list
### enumerator eMbxTferType_COE_GETOBDESC
CoE Get object description
### enumerator eMbxTferType_COE_GETENTRYDESC
CoE Get object entry description
### enumerator eMbxTferType_COE_EMERGENCY
CoE emergency request
### enumerator eMbxTferType_COE_RX_PDO
CoE RxPDO
### enumerator eMbxTferType_FOE_FILE_UPLOAD
FoE upload
### enumerator eMbxTferType_FOE_FILE_DOWNLOAD
FoE download
### enumerator eMbxTferType_SOE_READREQUEST
SoE read request
### enumerator eMbxTferType_SOE_READRESPONSE
SoE read response
### enumerator eMbxTferType_SOE_WRITEREQUEST
SoE write request
### enumerator eMbxTferType_SOE_WRITERESPONSE
SoE write response
### enumerator eMbxTferType_SOE_NOTIFICATION
SoE notification
### enumerator eMbxTferType_SOE_EMERGENCY
SoE emergency
### enumerator eMbxTferType_VOE_MBX_READ
VoE read
### enumerator eMbxTferType_VOE_MBX_WRITE
VoE write
### enumerator eMbxTferType_AOE_READ
AoE read
### enumerator eMbxTferType_AOE_WRITE
AoE write
### enumerator eMbxTferType_AOE_READWRITE
AoE read/write
### enumerator eMbxTferType_AOE_WRITECONTROL
AoE write control
### enumerator eMbxTferType_RAWMBX
Raw mbx
### enumerator eMbxTferType_FOE_SEG_DOWNLOAD
FoE segmented download
### enumerator eMbxTferType_FOE_SEG_UPLOAD
FoE segmented upload
### enumerator eMbxTferType_S2SMBX
S2S mbx
### enumerator eMbxTferType_FOE_UPLOAD_REQ
FoE upload request
### enumerator eMbxTferType_FOE_DOWNLOAD_REQ
FoE download request
### enumerator eMbxTferType_EOE_SEND_FRAME
EoE send frame
### enumerator eMbxTferType_EOE_RECEIVE_FRAME
EoE receive frame
### enumerator eMbxTferType_EOE_SET_IP
EoE set IP address
### union EC_T_MBX_DATA
*#include *
### Public Members
### [EC_T_AOE_CMD_RESPONSE](mbx_aoe.html.md#_CPPv421EC_T_AOE_CMD_RESPONSE) AoE_Response
AoE
### [EC_T_MBX_DATA_COE](mbx_coe.html.md#_CPPv417EC_T_MBX_DATA_COE) CoE
CoE
### [EC_T_COE_ODLIST](mbx_coe.html.md#_CPPv415EC_T_COE_ODLIST) CoE_ODList
CoE Object Dictionary list
### [EC_T_COE_OBDESC](mbx_coe.html.md#_CPPv415EC_T_COE_OBDESC) CoE_ObDesc
CoE object description
### [EC_T_COE_ENTRYDESC](mbx_coe.html.md#_CPPv418EC_T_COE_ENTRYDESC) CoE_EntryDesc
CoE entry description
### [EC_T_COE_EMERGENCY](mbx_coe.html.md#_CPPv418EC_T_COE_EMERGENCY) CoE_Emergency
CoE emergency data
### [EC_T_MBX_DATA_COE_INITCMD](mbx_coe.html.md#_CPPv425EC_T_MBX_DATA_COE_INITCMD) CoE_InitCmd
CoE InitCmd
### [EC_T_MBX_DATA_FOE](mbx_foe.html.md#_CPPv417EC_T_MBX_DATA_FOE) FoE
FoE
### EC_T_MBX_DATA_FOE_REQ FoE_Request
FoE request
### EC_T_MBX_DATA_SOE SoE
SoE
### EC_T_SOE_NOTIFICATION SoE_Notification
SoE notification request
### EC_T_SOE_EMERGENCY SoE_Emergency
SoE emergency request
#### SEE ALSO
EC-Master Class A about AoE, FoE and VoE mailbox protocols.
## emMbxTferAbort
### static [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) ecatMbxTferAbort([EC_T_MBXTFER](#_CPPv412EC_T_MBXTFER) \*pMbxTfer)
### [EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) emMbxTferAbort([EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwInstanceID, [EC_T_MBXTFER](#_CPPv412EC_T_MBXTFER) \*pMbxTfer)
Abort a running mailbox transfer.
This function may not be called from within the JobTask’s context.
* **Parameters:**
* **dwInstanceID** – [in] Instance ID (Multiple EtherCAT Network Support)
* **pMbxTfer** – [in] Mailbox transfer object created with emMbxTferCreate
* **Returns:**
[EC_E_NOERROR](error-codes_generic.html.md#d3/d2f/group___e_c___e_r_r_o_r___c_o_d_e_s___g_e_n_e_r_i_c_1ga8c8419c32e88e73d940a4501fe427116) if successful
Currently only supported for FoE Transfer, CoE Download and CoE Upload.
## emMbxTferDelete
### static EC_T_VOID ecatMbxTferDelete([EC_T_MBXTFER](#_CPPv412EC_T_MBXTFER) \*pMbxTfer)
### EC_T_VOID emMbxTferDelete([EC_T_DWORD](toc_api.html.md#_CPPv410EC_T_DWORD) dwInstanceID, [EC_T_MBXTFER](#_CPPv412EC_T_MBXTFER) \*pMbxTfer)
Deletes a mailbox transfer object.
A transfer object may only be deleted if it is in the Idle state.
* **Parameters:**
* **dwInstanceID** – [in] Instance ID (Multiple EtherCAT Network Support)
* **pMbxTfer** – [in] Mailbox transfer object created with emMbxTferCreate
* **Returns:**
[EC_E_NOERROR](error-codes_generic.html.md#d3/d2f/group___e_c___e_r_r_o_r___c_o_d_e_s___g_e_n_e_r_i_c_1ga8c8419c32e88e73d940a4501fe427116) or error code
## emNotify - EC_NOTIFY_MBOXRCV
Indicates a mailbox transfer completion.
**emNotify - EC_NOTIFY_MBOXRCV**
: **Parameter**
: * `pbyInBuf`: [in] Pointer to a structure of type EC_T_MBXTFER, containing the corresponding mailbox transfer object
* `dwInBufSize`: [in] Size of the transfer object provided at pbyInBuf in bytes
* `pbyOutBuf`: [out] Should be set to EC_NULL
* `dwOutBufSize`: [in] Should be set to 0
* `pdwNumOutData`: [out] Should be set to EC_NULL
The element [`EC_T_MBXTFER::dwClntId`](#_CPPv4N12EC_T_MBXTFER8dwClntIdE) contains the corresponding ID of the client that is notified, the corresponding transfer ID can be found in [`EC_T_MBXTFER::dwTferId`](#_CPPv4N12EC_T_MBXTFER8dwTferIdE). The transfer result is stored in [`EC_T_MBXTFER::dwErrorCode`](#_CPPv4N12EC_T_MBXTFER11dwErrorCodeE).
On error [`EC_T_MBXTFER::eTferStatus`](#_CPPv4N12EC_T_MBXTFER11eTferStatusE) is [`eMbxTferStatus_TferReqError`](#_CPPv4N19EC_T_MBXTFER_STATUS27eMbxTferStatus_TferReqErrorE), on success [`eMbxTferStatus_TferDone`](#_CPPv4N19EC_T_MBXTFER_STATUS23eMbxTferStatus_TferDoneE). In order to reuse the transfer object the application must set it back to [`eMbxTferStatus_Idle`](#_CPPv4N19EC_T_MBXTFER_STATUS19eMbxTferStatus_IdleE).
The [`EC_T_MBXTFER::eMbxTferType`](#_CPPv4N12EC_T_MBXTFER12eMbxTferTypeE) element determines the mailbox transfer type (e.g. [`eMbxTferType_COE_SDO_DOWNLOAD`](#_CPPv4N17EC_T_MBXTFER_TYPE29eMbxTferType_COE_SDO_DOWNLOADE) for a completion of a CoE SDO download transfer).