# EC-Master DotNet

> EC-Master DotNet documentation


2026-Oct-14, acontis technologies GmbH

## Pages

- [.NET Programming Interface](index.html.md): Main documentation page
- [Introduction](introduction.html.md): The .NET Wrapper provides a .NET interface to use EC-Master, EC-Monitor, EC-Simulator and RAS Client...
- [Programmers Guide](programmers-guide.html.md): There is currently 1 script available:
- [Application programming interface, reference](api.html.md): Function prototypes, definitions etc. of the API can be found in `CEcWrapperDotNet.cs` and `CEcWrapp...
- [CEcWrapperDotNet](api_wrapper.html.md): Subclassed by EcWrapperDotNet.CEcMasterMbxGatewayClientDotNet, EcWrapperDotNet.CEcMasterMbxGatewaySe...
- [Types](api_types.html.md): Abstract initalization parameters.
- [Error Codes](api_error-codes.html.md): summary> Specifies EtherCAT errors codes.
- [Examples](examples.html.md): public void CoeSdoUploadExample()
- [FAQ](faq.html.md): I installed .NET and the demo crashes with strange errors. What can I do?

---

For more comprehensive documentation, see [llms-full.txt](llms-full.txt)