# Error Codes ### *enum* EcWrapperDotNet.ECError summary> Specifies EtherCAT errors codes. *Values:* ### EC_NOERROR 0x00000000: No Error ### EC_ERROR 0x98110000: Unspecific Error ### EMRAS_ERROR 0x98110180: Unspecific RAS Error ### EC_NOTSUPPORTED 0x98110001: APP: Feature not supported (e.g. function or property not available) ### EC_INVALIDINDEX 0x98110002: APP: Invalid index (e.g. CoE: invalid SDO index) ### EC_INVALIDOFFSET 0x98110003: ISW: Invalid offset (e.g. invalid offset while accessing Process Data Image) ### EC_CANCEL 0x98110004: APP: Cancel (e.g. EtherCAT stack should abort current mailbox transfer) ### EC_INVALIDSIZE 0x98110005: APP: Invalid size ### EC_INVALIDDATA 0x98110006: ISW: Invalid data (multiple error sources) ### EC_NOTREADY 0x98110007: ISW: Not ready (multiple error sources) ### EC_BUSY 0x98110008: APP: Busy (e.g. EtherCAT stack is currently busy and not available to process the API request. The function may be called again later) ### EC_ACYC_FRM_FREEQ_EMPTY 0x98110009: ISW: Cannot queue acyclic EtherCAT command (Acyclic command queue is full. Possible solution: Increase of configuration value dwMaxQueuedEthFrames) ### EC_NOMEMORY 0x9811000A: CFG: No memory left (e.g. memory full / fragmented)) ### EC_INVALIDPARM 0x9811000B: APP: Invalid parameter (e.g. API function called with erroneous parameter set) ### EC_NOTFOUND 0x9811000C: APP: Not found (e.g. Network Information File ENI not found or API called with invalid slave ID) ### EC_DUPLICATE 0x9811000D: ISW: Duplicated fixed address detected (handled internally) ### EC_INVALIDSTATE 0x9811000E: ISW: Invalid state (EtherCAT stack not initialized or not configured) ### EC_TIMER_LIST_FULL 0x9811000F: ISW: Cannot add slave to timer list (slave timer list full) ### EC_TIMEOUT 0x98110010: Timeout ### EC_OPENFAILED 0x98110011: ISW: Open failed ### EC_SENDFAILED 0x98110012: LLA: Frame send failed ### EC_INSERTMAILBOX 0x98110013: CFG: Insert Mailbox error (internal limit MAX_QUEUED_COE_CMDS: 20) ### EC_INVALIDCMD 0x98110014: ISW: Invalid Command (Unknown mailbox command code) ### EC_UNKNOWN_MBX_PROTOCOL 0x98110015: ISW: Unknown Mailbox Protocol Command (Unknown Mailbox protocol or mailbox command with unknown protocol association) ### EC_ACCESSDENIED 0x98110016: ISW: Access Denied (e.g. master internal software error) ### EC_IDENTIFICATIONFAILED 0x98110017: ENI: Identification failed (e.g. identification command failed) ### EC_LOCK_CREATE_FAILED 0x98110018: SYS: Create lock failed (e.g. OsCreateLockTyped failed) ### EC_VERSION_MISMATCH 0x98110019: APP: Version mismatch for loaded library ### EC_PRODKEY_INVALID 0x9811001A: CFG: Product Key Invalid (e.g. application using protected version of the stack, which stops operation after the evaluation time limit reached if a license is not provided) ### EC_WRONG_FORMAT 0x9811001B: ENI: Wrong configuration format (e.g. Network information file empty or malformed), SLV: Malformed EEPROM content ### EC_FEATURE_DISABLED 0x9811001C: APP: Feature disabled (e.g. Application tried to perform a missing or disabled API function) ### EC_SHADOW_MEMORY 0x9811001D: Shadow memory requested in wrong mode ### EC_BUSCONFIG_MISMATCH 0x9811001E: ENI: Bus configuration mismatch (e.g. Network information file and currently connected bus topology does not match) ### EC_CONFIGDATAREAD 0x9811001F: ENI: Error reading configuration file (e.g. Network information file could not be read) ### EC_ENI_NO_SAFEOP_OP_SUPPORT 0x98110020: Configuration doesn’t support SAFEOP and OP requested state ### EC_XML_CYCCMDS_MISSING 0x98110021: ENI: Cyclic commands are missing (e.g. Network information file does not contain cyclic commands) ### EC_XML_ALSTATUS_READ_MISSING 0x98110022: ENI: AL_STATUS register read missing in XML file for at least one state (e.g. Read of AL Status register is missing in cyclic part of given network information file) ### EC_MCSM_FATAL_ERROR 0x98110023: ISW: Fatal internal McSm (master control state machine is in an undefined state) ### EC_SLAVE_ERROR 0x98110024: SLV: Slave error (e.g. A slave error was detected. See also EC_NOTIFY_STATUS_SLAVE_ERROR and EC_NOTIFY_SLAVE_ERROR_STATUS_INFO) ### EC_FRAME_LOST 0x98110025: SLV: Frame lost, IDX mismatch (EtherCAT frame(s) lost on bus, means the response was not received. In case this error shows frequently a problem with the wiring could be the cause) ### EC_CMD_MISSING 0x98110026: SLV: At least one EtherCAT command is missing in the received frame (e.g. received EtherCAT frame incomplete) ### EC_CYCCMD_WKC_ERROR 0x98110027: Cyclic command WKC error ### EC_INVALID_DCL_MODE 0x98110028: APP: IOCTL EC_IOCTL_DC_LATCH_REQ_LTIMVALS invalid in DCL auto read mode (this function cannot be used if DC Latching is running in mode “Auto Read”) ### EC_AI_ADDRESS 0x98110029: SLV: Auto increment address increment mismatch (e.g. Network information file and bus topology doesn’t match any more. Error shows only, if an already recognized slave isn’t present any more) ### EC_INVALID_SLAVE_STATE 0x9811002A: APP: Slave in invalid state, e.g. not in OP (API not callable in this state) (mailbox commands are not allowed in current slave state) ### EC_SLAVE_NOT_ADDRESSABLE 0x9811002B: SLV: Station address lost (or slave missing) - FPRD to AL_STATUS failed (e.g. Slave had a power cycle) ### EC_CYC_CMDS_OVERFLOW 0x9811002C: ENI: Too many cyclic commands in XML configuration file (e.g. EC_T_INIT_MASTER_PARMS.dwMaxAcycFramesQueued too small) ### EC_LINK_DISCONNECTED 0x9811002D: SLV: Ethernet link cable disconnected (e.g. EtherCAT bus segment not connected to network interface) ### EC_MASTERCORE_INACCESSIBLE 0x9811002E: RAS: Simulator core not accessible (e.g. Connection to remote server was terminated or simulator instance has been stopped on remote side) ### EC_COE_MBXSND_WKC_ERROR 0x9811002F: SLV: CoE mailbox send: working counter (e.g. CoE mailbox couldn’t be read on slave, slave didn’t read out mailbox since last write) ### EC_COE_MBXRCV_WKC_ERROR 0x98110030: SLV: CoE mailbox receive: working counter (e.g. CoE mailbox couldn’t be read from slave) ### EC_NO_MBX_SUPPORT 0x98110031: APP: No mailbox support (e.g. Slave does not support mailbox access) ### EC_NO_COE_SUPPORT 0x98110032: ENI: CoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware) ### EC_NO_EOE_SUPPORT 0x98110033: ENI: EoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware) ### EC_NO_FOE_SUPPORT 0x98110034: ENI: FoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware) ### EC_NO_SOE_SUPPORT 0x98110035: ENI: SoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware) ### EC_NO_VOE_SUPPORT 0x98110036: ENI: VoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware) ### EC_EVAL_VIOLATION 0x98110037: ENI: Configuration violates Evaluation limits (obsolete) ### EC_EVAL_EXPIRED 0x98110038: CFG: Evaluation Time limit reached (e.g. License not provided and evaluation period (1 hour) of protected version exceeded) ### EC_LICENSE_MISSING 0x98110039: License key invalid or missing ### EC_SDO_ABORTCODE_FIRST EC_SDO_ABORTCODE_FIRST. ### EC_SDO_ABORTCODE_TOGGLE 0x98110040: SLV: SDO: Toggle bit not alternated (CoE abort code 0x05030000 of slave) ### EC_SDO_ABORTCODE_TIMEOUT 0x98110041: SLV: SDO: Protocol timed out (CoE abort code 0x05040000 of slave) ### EC_SDO_ABORTCODE_CCS_SCS 0x98110042: SLV: SDO: Client/server command specifier not valid or unknown (CoE abort code 0x05040001 of slave) ### EC_SDO_ABORTCODE_BLK_SIZE 0x98110043: SLV: SDO: Invalid block size (block mode only) (CoE abort code 0x05040002 of slave) ### EC_SDO_ABORTCODE_SEQNO 0x98110044: SLV: SDO: Invalid sequence number (block mode only) (CoE abort code 0x05040003 of slave) ### EC_SDO_ABORTCODE_CRC 0x98110045: SLV: SDO: CRC error (block mode only) (CoE abort code 0x05040004 of slave) ### EC_SDO_ABORTCODE_MEMORY 0x98110046: SLV: SDO: Out of memory (CoE abort code 0x05040005 of slave) ### EC_SDO_ABORTCODE_ACCESS 0x98110047: SLV: SDO: Unsupported access to an object (CoE abort code 0x06010000 of slave) ### EC_SDO_ABORTCODE_WRITEONLY 0x98110048: SLV: SDO: Attempt to read a write only object (CoE abort code 0x06010001 of slave) ### EC_SDO_ABORTCODE_READONLY 0x98110049: SLV: SDO: Attempt to write a read only object (CoE abort code 0x06010002 of slave) ### EC_SDO_ABORTCODE_INDEX 0x9811004A: SLV: SDO: Object does not exist in the object dictionary (CoE abort code 0x06020000 of slave) ### EC_SDO_ABORTCODE_PDO_MAP 0x9811004B: SLV: SDO: Object cannot be mapped to the PDO (CoE abort code 0x06040041 of slave) ### EC_SDO_ABORTCODE_PDO_LEN 0x9811004C: SLV: SDO: The number and length of the objects to be mapped would exceed PDO length (CoE abort code 0x06040042 of slave) ### EC_SDO_ABORTCODE_P_INCOMP 0x9811004D: SLV: SDO: General parameter incompatibility reason (CoE abort code 0x06040043 of slave) ### EC_SDO_ABORTCODE_I_INCOMP 0x9811004E: SLV: SDO: General internal incompatibility in the device (CoE abort code 0x06040047 of slave) ### EC_SDO_ABORTCODE_HARDWARE 0x9811004F: SLV: SDO: Access failed due to a hardware error (CoE abort code 0x06060000 of slave) ### EC_SDO_ABORTCODE_DATA_LENGTH_NOT_MATCH 0x98110050: SLV: SDO: Data type does not match, length of service parameter does not match (CoE abort code 0x06070010 of slave) ### EC_SDO_ABORTCODE_DATA_LENGTH_TOO_HIGH 0x98110051: SLV: SDO: Data type does not match, length of service parameter too high (CoE abort code 0x06070012 of slave) ### EC_SDO_ABORTCODE_DATA_LENGTH_TOO_LOW 0x98110052: SLV: SDO: Data type does not match, length of service parameter too low (CoE abort code 0x06070013 of slave) ### EC_SDO_ABORTCODE_OFFSET 0x98110053: SLV: SDO: Sub-index does not exist (CoE abort code 0x06090011 of slave) ### EC_SDO_ABORTCODE_VALUE_RANGE 0x98110054: SLV: SDO: Value range of parameter exceeded (only for write access) (CoE abort code 0x06090030 of slave) ### EC_SDO_ABORTCODE_VALUE_TOO_HIGH 0x98110055: SLV: SDO: Value of parameter written too high (CoE abort code 0x06090031 of slave) ### EC_SDO_ABORTCODE_VALUE_TOO_LOW 0x98110056: SLV: SDO: Value of parameter written too low (CoE abort code 0x06090032 of slave) ### EC_SDO_ABORTCODE_MINMAX 0x98110057: SLV: SDO: Maximum value is less than minimum value (CoE abort code 0x06090036 of slave) ### EC_SDO_ABORTCODE_GENERAL 0x98110058: SLV: SDO: General error (CoE abort code 0x08000000 of slave) ### EC_SDO_ABORTCODE_TRANSFER 0x98110059: SLV: SDO: Data cannot be transferred or stored to the application (CoE abort code 0x08000020 of slave) ### EC_SDO_ABORTCODE_TRANSFER_LOCAL_CONTROL 0x9811005A: SLV: SDO: Data cannot be transferred or stored to the application because of local control (CoE abort code 0x08000021 of slave) ### EC_SDO_ABORTCODE_TRANSFER_DEVICE_STATE 0x9811005B: SLV: SDO: Data cannot be transferred or stored to the application because of the present device state (CoE abort code 0x08000022 of slave) ### EC_SDO_ABORTCODE_DICTIONARY 0x9811005C: SLV: SDO: Object dictionary dynamic generation fails or no object dictionary is present (e.g. object dictionary is generated from file and generation fails because of an file error) (CoE abort code 0x08000023 of slave) ### EC_SDO_ABORTCODE_UNKNOWN 0x9811005D: SLV: SDO: Unknown code (Unknown CoE abort code of slave) ### EC_SDO_ABORTCODE_MODULE_ID_LIST_NOT_MATCH 0x9811005E: Detected Module Ident List (0xF030) and Configured Module Ident list (0xF050) does not match ### EC_SDO_ABORTCODE_LAST EC_SDO_ABORTCODE_LAST. ### EC_FOE_ERRCODE_NOTDEFINED 0x98110060: SLV: ERROR FoE: not defined (FoE Error Code 0 (0x8000) of slave) ### EC_FOE_ERRCODE_NOTFOUND 0x98110061: SLV: ERROR FoE: not found (FoE Error Code 1 (0x8001) of slave) ### EC_FOE_ERRCODE_ACCESS 0x98110062: SLV: ERROR FoE: access denied (FoE Error Code 2 (0x8002) of slave) ### EC_FOE_ERRCODE_DISKFULL 0x98110063: SLV: ERROR FoE: disk full (FoE Error Code 3 (0x8003) of slave) ### EC_FOE_ERRCODE_ILLEGAL 0x98110064: SLV: ERROR FoE: illegal (FoE Error Code 4 (0x8004) of slave) ### EC_FOE_ERRCODE_PACKENO 0x98110065: SLV: ERROR FoE: packet number wrong (FoE Error Code 5 (0x8005) of slave) ### EC_FOE_ERRCODE_EXISTS 0x98110066: SLV: ERROR FoE: already exists (FoE Error Code 6 (0x8006) of slave) ### EC_FOE_ERRCODE_NOUSER 0x98110067: SLV: ERROR FoE: no user (FoE Error Code 7 (0x8007) of slave) ### EC_FOE_ERRCODE_BOOTSTRAPONLY 0x98110068: SLV: ERROR FoE: bootstrap only (FoE Error Code 8 (0x8008) of slave) ### EC_FOE_ERRCODE_NOTINBOOTSTRAP 0x98110069: SLV: ERROR FoE: Downloaded file name is not valid in Bootstrap state (FoE Error Code 9 (0x8009) of slave) ### EC_FOE_ERRCODE_INVALIDPASSWORD 0x9811006A: SLV: ERROR FoE: no rights (FoE Error Code 10 (0x800A) of slave) ### EC_FOE_ERRCODE_PROGERROR 0x9811006B: SLV: ERROR FoE: program error (FoE Error Code 11 (0x800B) of slave) ### EC_FOE_ERRCODE_INVALID_CHECKSUM 0x9811006C: FoE: Wrong checksum ### EC_FOE_ERRCODE_INVALID_FIRMWARE 0x9811006D: SLV: ERROR FoE: Firmware does not fit for Hardware (FoE Error Code 13 (0x800D) of slave) ### EC_FOE_ERRCODE_NO_FILE 0x9811006F: SLV: ERROR FoE: No file to read (FoE Error Code 15 (0x800F) of slave) ### EC_CFGFILENOTFOUND 0x98110070: CFG: Network configuration file not found (e.g. path to configuration file (XML) was wrong or the file is not available) ### EC_EEPROMREADERROR 0x98110071: SLV: Command error while EEPROM upload (read slave EEPROM) ### EC_EEPROMWRITEERROR 0x98110072: SLV: Command error while EEPROM download (write slave EEPROM) ### EC_XML_CYCCMDS_SIZEMISMATCH 0x98110073: ENI: Cyclic command wrong size (too long) (size in network configuration file (XML) does not match size of process data) ### EC_XML_INVALID_INP_OFF 0x98110074: ENI: Invalid input offset in cyclic command, please check InputOffs ### EC_XML_INVALID_OUT_OFF 0x98110075: ENI: Invalid output offset in cyclic command, please check OutputOffs ### EC_PORTCLOSE 0x98110076: Port close failed ### EC_PORTOPEN 0x98110077: Port open failed ### EC_SOE_ERRORCODE_INVALID_ACCESS 0x98110078: ERROR SoE: Invalid access to element 0 ### EC_SOE_ERRORCODE_NOT_EXIST 0x98110079: ERROR SoE: Does not exist ### EC_SOE_ERRORCODE_INVL_ACC_ELEM1 0x9811007A: ERROR SoE: Invalid access to element 1 ### EC_SOE_ERRORCODE_NAME_NOT_EXIST 0x9811007B: ERROR SoE: Name does not exist ### EC_SOE_ERRORCODE_NAME_UNDERSIZE 0x9811007C: ERROR SoE: Name undersize in transmission ### EC_SOE_ERRORCODE_NAME_OVERSIZE 0x9811007D: ERROR SoE: Name oversize in transmission ### EC_SOE_ERRORCODE_NAME_UNCHANGE 0x9811007E: ERROR SoE: Name unchangeable ### EC_SOE_ERRORCODE_NAME_WR_PROT 0x9811007F: ERROR SoE: Name currently write-protected ### EC_SOE_ERRORCODE_UNDERS_TRANS 0x98110080: ERROR SoE: Attribute undersize in transmission ### EC_SOE_ERRORCODE_OVERS_TRANS 0x98110081: ERROR SoE: Attribute oversize in transmission ### EC_SOE_ERRORCODE_ATTR_UNCHANGE 0x98110082: ERROR SoE: Attribute unchangeable ### EC_SOE_ERRORCODE_ATTR_WR_PROT 0x98110083: ERROR SoE: Attribute currently write-protected ### EC_SOE_ERRORCODE_UNIT_NOT_EXIST 0x98110084: ERROR SoE: Unit does not exist ### EC_SOE_ERRORCODE_UNIT_UNDERSIZE 0x98110085: ERROR SoE: Unit undersize in transmission ### EC_SOE_ERRORCODE_UNIT_OVERSIZE 0x98110086: ERROR SoE: Unit oversize in transmission ### EC_SOE_ERRORCODE_UNIT_UNCHANGE 0x98110087: ERROR SoE: Unit unchangeable ### EC_SOE_ERRORCODE_UNIT_WR_PROT 0x98110088: ERROR SoE: Unit currently write-protected ### EC_SOE_ERRORCODE_MIN_NOT_EXIST 0x98110089: ERROR SoE: Minimum input value does not exist ### EC_SOE_ERRORCODE_MIN_UNDERSIZE 0x9811008A: ERROR SoE: Minimum input value undersize in transmission ### EC_SOE_ERRORCODE_MIN_OVERSIZE 0x9811008B: ERROR SoE: Minimum input value oversize in transmission ### EC_SOE_ERRORCODE_MIN_UNCHANGE 0x9811008C: ERROR SoE: Minimum input value unchangeable ### EC_SOE_ERRORCODE_MIN_WR_PROT 0x9811008D: ERROR SoE: Minimum input value currently write-protected ### EC_SOE_ERRORCODE_MAX_NOT_EXIST 0x9811008E: ERROR SoE: Maximum input value does not exist ### EC_SOE_ERRORCODE_MAX_UNDERSIZE 0x9811008F: ERROR SoE: Maximum input value undersize in transmission ### EC_SOE_ERRORCODE_MAX_OVERSIZE 0x98110090: ERROR SoE: Maximum input value oversize in transmission ### EC_SOE_ERRORCODE_MAX_UNCHANGE 0x98110091: ERROR SoE: Maximum input value unchangeable ### EC_SOE_ERRORCODE_MAX_WR_PROT 0x98110092: ERROR SoE: Maximum input value currently write-protected ### EC_SOE_ERRORCODE_DATA_NOT_EXIST 0x98110093: ERROR SoE: Data item does not exist ### EC_SOE_ERRORCODE_DATA_UNDERSIZE 0x98110094: ERROR SoE: Data item undersize in transmission ### EC_SOE_ERRORCODE_DATA_OVERSIZE 0x98110095: ERROR SoE: Data item oversize in transmission ### EC_SOE_ERRORCODE_DATA_UNCHANGE 0x98110096: ERROR SoE: Data item unchangeable ### EC_SOE_ERRORCODE_DATA_WR_PROT 0x98110097: ERROR SoE: Data item currently write-protected ### EC_SOE_ERRORCODE_DATA_MIN_LIMIT 0x98110098: ERROR SoE: Data item less than minimum input value limit ### EC_SOE_ERRORCODE_DATA_MAX_LIMIT 0x98110099: ERROR SoE: Data item exceeds maximum input value limit ### EC_SOE_ERRORCODE_DATA_INCOR 0x9811009A: ERROR SoE: Data item incorrect ### EC_SOE_ERRORCODE_PASWD_PROT 0x9811009B: ERROR SoE: Data item protected by password ### EC_SOE_ERRORCODE_TEMP_UNCHANGE 0x9811009C: ERROR SoE: Data item temporary unchangeable (in AT or MDT) ### EC_SOE_ERRORCODE_INVL_INDIRECT 0x9811009D: ERROR SoE: Invalid indirect ### EC_SOE_ERRORCODE_TEMP_UNCHANGE1 0x9811009E: ERROR SoE: Data item temporary unchangeable (parameter or opmode) ### EC_SOE_ERRORCODE_ALREADY_ACTIVE 0x9811009F: ERROR SoE: Command already active ### EC_SOE_ERRORCODE_NOT_INTERRUPT 0x98110100: ERROR SoE: Command not interruptible ### EC_SOE_ERRORCODE_CMD_NOT_AVAIL 0x98110101: ERROR SoE: Command not available (in this phase) ### EC_SOE_ERRORCODE_CMD_NOT_AVAIL1 0x98110102: ERROR SoE: Command not available (invalid parameter) ### EC_SOE_ERRORCODE_DRIVE_NO 0x98110103: ERROR SoE: Response drive number not identical with requested drive number ### EC_SOE_ERRORCODE_IDN 0x98110104: ERROR SoE: Response IDN not identical with requested IDN ### EC_SOE_ERRORCODE_FRAGMENT_LOST 0x98110105: ERROR SoE: At least one fragment lost ### EC_SOE_ERRORCODE_BUFFER_FULL 0x98110106: ERROR SoE: RX buffer full (EtherCAT call with to small data-buffer) ### EC_SOE_ERRORCODE_NO_DATA 0x98110107: ERROR SoE: No data state ### EC_SOE_ERRORCODE_NO_DEFAULT_VALUE 0x98110108: ERROR SoE: No default value ### EC_SOE_ERRORCODE_DEFAULT_LONG 0x98110109: ERROR SoE: Default value transmission too long ### EC_SOE_ERRORCODE_DEFAULT_WP 0x9811010A: ERROR SoE: Default value cannot be changed, read only ### EC_SOE_ERRORCODE_INVL_DRIVE_NO 0x9811010B: ERROR SoE: Invalid drive number ### EC_SOE_ERRORCODE_GENERAL_ERROR 0x9811010C: ERROR SoE: General error ### EC_SOE_ERRCODE_NO_ELEM_ADR 0x9811010D: ERROR SoE: No element addressed ### EC_SLAVE_NOT_PRESENT 0x9811010E: APP / SLV: command not executed (slave not present on bus) (e.g. slave disappeared or was never present) ### EC_NO_FOE_SUPPORT_BS 0x9811010F: APP: ERROR FoE: Protocol not supported in boot strap (e.g. Application requested FoE in Bootstrap although slave does not support this) ### EC_EEPROMRELOADERROR 0x98110110: Command error while EEPROM reload ### EC_SLAVECTRLRESETERROR 0x98110111: Command error while Reset Slave Controller ### EC_SYSDRIVERMISSING 0x98110112: SYS: Cannot open system driver (e.g. system driver was not loaded) ### EC_BUSCONFIG_TOPOCHANGE 0x9811011E: Bus configuration not detected, Topology changed (e.g. Topology changed while scanning bus) ### EC_EOE_MBX_WKC_ERROR 0x9811011F: EoE: Mailbox receive: working counter ### EC_FOE_MBX_WKC_ERROR 0x98110120: FoE: Mailbox receive: working counter ### EC_SOE_MBX_WKC_ERROR 0x98110121: SoE: mailbox receive: working counter ### EC_AOE_MBX_WKC_ERROR 0x98110122: AoE: Mailbox receive: working counter ### EC_VOE_MBX_WKC_ERROR 0x98110123: SLV: VoE mailbox send: working counter (VoE mailbox couldn’t be written) ### EC_EEPROMASSIGNERROR 0x98110124: SLV: EEPROM assignment failed ### EC_MBX_ERROR_TYPE 0x98110125: SLV: Unknown mailbox error code received in mailbox ### EC_REDLINEBREAK 0x98110126: SLV: Redundancy line break (e.g. cable break between slaves or between EtherCAT network adapter and first slave) ### EC_XML_INVALID_CMD_WITH_RED 0x98110127: ENI: Invalid EtherCAT command in cyclic frame with redundancy (e.g. BRW commands are not allowed with redundancy) ### EC_XML_PREV_PORT_MISSING 0x98110128: ENI: -tag is missing (e.g. if the auto increment address is not the first slave on the bus we check if a previous port tag OR a hot connect tag is available) ### EC_XML_DC_CYCCMDS_MISSING 0x98110129: DC enabled and DC cyclic commands missing (e.g. access to 0x0900) ### EC_DLSTATUS_IRQ_TOPOCHANGED 0x98110130: SLV: Data link (DL) status interrupt because of changed topology (automatically handled by master) ### EC_PTS_IS_NOT_RUNNING 0x98110131: PTS: Pass Through Server is not running (Pass-Through-Server was tried to be enabled/disabled or stopped without being started) ### EC_PTS_IS_RUNNING 0x98110132: PTS: Pass Through Server is running (obsolete, replaced by EC_E_ADS_IS_RUNNING) ### EC_ADS_IS_RUNNING 0x98110132: PTS: ADS adapter (Pass Through Server) is running (API call conflicts with ADS state (running)) ### EC_PTS_THREAD_CREATE_FAILED 0x98110133: PTS: Could not start the Pass Through Server ### EC_PTS_SOCK_BIND_FAILED 0x98110134: PTS: The Pass Through Server could not bind the IP address with a socket (e.g. Possibly because the IPaddress (and Port) is already in use or the IP-address does not exist) ### EC_PTS_NOT_ENABLED 0x98110135: PTS: The Pass Through Server is running but not enabled ### EC_PTS_LL_MODE_NOT_SUPPORTED 0x98110136: PTS: The Link Layer mode is not supported by the Pass Through Server (e.g. The Master is running in interrupt mode but the Pass-Through-Server only supports polling mode) ### EC_VOE_NO_MBX_RECEIVED 0x98110137: SLV: No VoE mailbox received yet from specific slave ### EC_DC_REF_CLOCK_SYNC_OUT_UNIT_DISABLED 0x98110138: DC (time loop control) unit of reference clock disabled ### EC_DC_REF_CLOCK_NOT_FOUND 0x98110139: SLV: Reference clock not found! May happen if reference clock is removed from network. ### EC_MBX_CMD_WKC_ERROR 0x9811013B: SLV: Mailbox command working counter error (e.g. Mailbox init command Retry Count exceeded) ### EC_NO_AOE_SUPPORT 0x9811013C: APP / SLV: AoE: Protocol not supported (e.g. Application calls AoE-API although not implemented at slave) ### EC_AOE_INV_RESPONSE_SIZE 0x9811013D: AoE: Invalid AoE response received ### EC_AOE_ERROR 0x9811013E: AoE: Common AoE device error ### EC_AOE_SRVNOTSUPP 0x9811013F: AoE: Service not supported by server ### EC_AOE_INVALIDGRP 0x98110140: AoE: Invalid index group ### EC_AOE_INVALIDOFFSET 0x98110141: AoE: Invalid index offset ### EC_AOE_INVALIDACCESS 0x98110142: AoE: Reading/writing not permitted ### EC_AOE_INVALIDSIZE 0x98110143: AoE: Parameter size not correct ### EC_AOE_INVALIDDATA 0x98110144: AoE: Invalid parameter value(s) ### EC_AOE_NOTREADY 0x98110145: AoE: Device not in a ready state ### EC_AOE_BUSY 0x98110146: AoE: Device busy ### EC_AOE_INVALIDCONTEXT 0x98110147: AoE: Invalid context ### EC_AOE_NOMEMORY 0x98110148: AoE: Out of memory ### EC_AOE_INVALIDPARM 0x98110149: AoE: Invalid parameter value(s) ### EC_AOE_NOTFOUND 0x9811014A: AoE: Not found ### EC_AOE_SYNTAX 0x9811014B: AoE: Syntax error in command or file ### EC_AOE_INCOMPATIBLE 0x9811014C: AoE: Objects do not match ### EC_AOE_EXISTS 0x9811014D: AoE: Object already exists ### EC_AOE_SYMBOLNOTFOUND 0x9811014E: AoE: Symbol not found ### EC_AOE_SYMBOLVERSIONINVALID 0x9811014F: AoE: Symbol version invalid ### EC_AOE_INVALIDSTATE 0x98110150: AoE: Server in invalid state ### EC_AOE_TRANSMODENOTSUPP 0x98110151: AoE: AdsTransMode not supported ### EC_AOE_NOTIFYHNDINVALID 0x98110152: AoE: Notification handle invalid ### EC_AOE_CLIENTUNKNOWN 0x98110153: AoE: Notification client not registered ### EC_AOE_NOMOREHDLS 0x98110154: AoE: No more notification handles ### EC_AOE_INVALIDWATCHSIZE 0x98110155: AoE: Size for watch to big ### EC_AOE_NOTINIT 0x98110156: AoE: Device not initialized ### EC_AOE_TIMEOUT 0x98110157: AoE: Device has a timeout ### EC_AOE_NOINTERFACE 0x98110158: AoE: Query interface failed ### EC_AOE_INVALIDINTERFACE 0x98110159: AoE: Wrong interface required ### EC_AOE_INVALIDCLSID 0x9811015A: AoE: Class ID invalid ### EC_AOE_INVALIDOBJID 0x9811015B: AoE: Object ID invalid ### EC_AOE_PENDING 0x9811015C: AoE: Request pending ### EC_AOE_ABORTED 0x9811015D: AoE: Request aborted ### EC_AOE_WARNING 0x9811015E: AoE: Signal warning ### EC_AOE_INVALIDARRAYIDX 0x9811015F: AoE: Invalid array index ### EC_AOE_SYMBOLNOTACTIVE 0x98110160: AoE: Symbol not active -> release handle and try again ### EC_AOE_ACCESSDENIED 0x98110161: AoE: Access denied ### EC_AOE_INTERNAL 0x98110162: AoE: Internal error ### EC_AOE_TARGET_PORT_NOT_FOUND 0x98110163: AoE: Target port not found ### EC_AOE_TARGET_MACHINE_NOT_FOUND 0x98110164: AoE: Target machine not found ### EC_AOE_UNKNOWN_CMD_ID 0x98110165: AoE: Unknown command ID ### EC_AOE_PORT_NOT_CONNECTED 0x98110166: AoE: Port not connected ### EC_AOE_INVALID_AMS_LENGTH 0x98110167: AoE: Invalid AMS length ### EC_AOE_INVALID_AMS_ID 0x98110168: AoE: invalid AMS Net ID ### EC_AOE_PORT_DISABLED 0x98110169: AoE: Port disabled ### EC_AOE_PORT_CONNECTED 0x9811016A: AoE: Port already connected ### EC_AOE_INVALID_AMS_PORT 0x9811016B: AoE: Invalid AMS port ### EC_AOE_NO_MEMORY 0x9811016C: AoE: No memory ### EC_AOE_VENDOR_SPECIFIC 0x9811016D: AoE: Vendor specific AoE device error ### EC_XML_AOE_NETID_INVALID 0x9811016E: ENI: AoE: Invalid NetID (e.g. Error from Configuration Tool) ### EC_MAX_BUS_SLAVES_EXCEEDED 0x9811016F: CFG: Error: Maximum number of bus slave has been exceeded (The maximum number of preallocated bus slave objects is too small. The maximum number can be adjusted by the master initialization parameter EC_T_INITMASTERPARMS.dwMaxBusSlaves) ### EC_MBXERR_SYNTAX 0x98110170: SLV: Mailbox error: Syntax of 6 octet Mailbox header is wrong (Slave error mailbox return value: 0x01) ### EC_MBXERR_UNSUPPORTEDPROTOCOL 0x98110171: SLV: Mailbox error: The Mailbox protocol is not supported (Slave error mailbox return value: 0x02) ### EC_MBXERR_INVALIDCHANNEL 0x98110172: SLV: Mailbox error: Field contains wrong value (Slave error mailbox return value: 0x03) ### EC_MBXERR_SERVICENOTSUPPORTED 0x98110173: SLV: Mailbox error: The addressed service in the mailbox protocol is not supported (Slave error mailbox return value: 0x04) ### EC_MBXERR_INVALIDHEADER 0x98110174: SLV: Mailbox error: The mailbox protocol header of the mailbox protocol is wrong (Slave error mailbox return value: 0x05) ### EC_MBXERR_SIZETOOSHORT 0x98110175: SLV: Mailbox error: Length of received mailbox data is too short (Slave error mailbox return value: 0x06) ### EC_MBXERR_NOMOREMEMORY 0x98110176: SLV: Mailbox error: Mailbox protocol can not be processed because of limited resources (Slave error mailbox return value: 0x07) ### EC_MBXERR_INVALIDSIZE 0x98110177: SLV: Mailbox error: The length of data is inconsistent (Slave error mailbox return value: 0x08) ### EC_DC_SLAVES_BEFORE_REF_CLOCK 0x98110178: ENI: Slaves with DC configured present on bus before reference clock (e.g. The first DC Slave was not configured as potential reference clock) ### EC_DATA_TYPE_CONVERSION_FAILED 0x98110179: Data type conversion failed ### EC_FOE_ERRCODE_MAX_FILE_SIZE 0x9811017A: APP: ERROR FoE: File is bigger than max file size (e.g. Slave returned more data than the buffer provided by application can store.) ### EC_LINE_CROSSED 0x9811017B: Line crossed (cabling wrong) ### EC_LINE_CROSSED_SLAVE_INFO 0x9811017C: Line crossed at slave (obsolete) ### EC_SOCKET_DISCONNECTED 0x9811017D: RAS: Socket disconnected (e.g. IP connection terminated or lost) ### EC_ADO_NOT_SUPPORTED 0x9811017E: SLV: ADO for slave identification not supported (e.g. Request ID mechanism (ADO 0x134) not supported by slave) ### EC_FRAMELOSS_AFTER_SLAVE 0x9811017F: Frameloss after Slave (opening port destroys communication) ### EC_ERROR_LAST EC_ERROR_LAST. ### EC_ERROR2 EC_ERROR2. ### EC_FOE_ERRCODE_FILE_HEAD_MISSING 0x98130001: SLV: ERROR FoE: File header does not exist (FoE Error Code 16 (0x8010) of slave) ### EC_FOE_ERRCODE_FLASH_PROBLEM 0x98130002: SLV: ERROR FoE: Flash problem (FoE Error Code 17 (0x8011) of slave) ### EC_FOE_ERRCODE_FILE_INCOMPATIBLE 0x98130003: SLV: ERROR FoE: File incompatible (FoE Error Code 18 (0x8012) of slave) ### EC_SDO_ABORTCODE_SI_NOT_WRITTEN 0x98130004: SLV: SDO: Sub Index cannot be written, SI0 must be 0 for write access (CoE abort code 0x06010003 of slave) ### EC_SDO_ABORTCODE_CA_TYPE_MISM 0x98130005: SLV: SDO: Complete access not supported for objects of variable length such as ENUM object types (CoE abort code 0x06010004 of slave) ### EC_SDO_ABORTCODE_OBJ_TOO_BIG 0x98130006: SLV: SDO: Object length exceeds mailbox size (CoE abort code 0x06010005 of slave) ### EC_SDO_ABORTCODE_PDO_MAPPED 0x98130007: SLV: SDO: Object mapped to RxPDO, SDO Download blocked (CoE abort code 0x06010006 of slave) ### EC_OEM_SIGNATURE_MISMATCH 0x98130008: ENI, OEM: Manufacturer signature mismatch ### EC_ENI_ENCRYPTION_WRONG_VERSION 0x98130009: ENI, OEM: ENI encryption algorithm version not supported ### EC_ENI_ENCRYPTED 0x9813000A: OEM: Loading encrypted ENI needs OEM key ### EC_OEM_KEY_MISMATCH 0x9813000B: RAS, APP: OEM key mismatch ### EC_OEM_KEY_MISSING 0x9813000C: APP: OEM key access needs OEM key set (e.g. Application must call esSetOemKey (HiL) or set EC_T_LINK_PARMS_SIMULATOR::qwOemKey (SiL)) ### EC_AOE_NO_RTIME 0x9813000D: AoE: No Rtime ### EC_AOE_LOCKED_MEMORY 0x9813000E: AoE: Allocation locked memory ### EC_AOE_MAILBOX 0x9813000F: AoE: Insert mailbox error ### EC_AOE_WRONG_HMSG 0x98130010: AoE: Wrong receive HMSG ### EC_AOE_BAD_TASK_ID 0x98130011: AoE: Bad task ID ### EC_AOE_NO_IO 0x98130012: AoE: No IO ### EC_AOE_UNKNOWN_AMS_COMMAND 0x98130013: AoE: Unknown ADS command ### EC_AOE_WIN32 0x98130014: AoE: Win 32 error ### EC_AOE_LOW_INSTALL_LEVEL 0x98130015: AoE: Low installation level ### EC_AOE_NO_DEBUG 0x98130016: AoE: No debug available ### EC_AOE_AMS_SYNC_WIN32 0x98130017: AoE: Sync Win 32 error ### EC_AOE_AMS_SYNC_TIMEOUT 0x98130018: AoE: Sync Timeout ### EC_AOE_AMS_SYNC_AMS 0x98130019: AoE: Sync AMS error ### EC_AOE_AMS_SYNC_NO_INDEX_MAP 0x9813001A: AoE: Sync no index map ### EC_AOE_TCP_SEND 0x9813001B: AoE: TCP send error ### EC_AOE_HOST_UNREACHABLE 0x9813001C: AoE: Host unreachable ### EC_AOE_INVALIDAMSFRAGMENT 0x9813001D: AoE: Invalid AMS fragment ### EC_AOE_NO_LOCKED_MEMORY 0x9813001E: AoE: No allocation locked memory ### EC_AOE_MAILBOX_FULL 0x9813001F: AoE: Mailbox full ### EC_S2SMBX_NOT_CONFIGURED 0x98130020: S2S: Not Configured ### EC_S2SMBX_NO_MEMORY 0x98130021: S2S: No Memory ### EC_S2SMBX_NO_DESCRIPTOR 0x98130022: S2S: No Descriptor ### EC_S2SMBX_DEST_SLAVE_NOT_FOUND 0x98130023: S2S: Destination Slave not found ### EC_MASTER_RED_STATE_INACTIVE 0x98130024: APP: Master Redundancy State is INACTIVE (e.g. API not allowed in current Master Redundancy State) ### EC_MASTER_RED_STATE_ACTIVE 0x98130025: APP: Master Redundancy State is ACTIVE (e.g. API not allowed in current Master Redundancy State) ### EC_JUNCTION_RED_LINE_BREAK 0x98130026: Junction redundancy line break ### EC_VALIDATION_ERROR 0x98130027: Validation error (validation data mismatch) ### EC_TIMEOUT_WAITING_FOR_DC 0x98130028: Timeout waiting for DC ### EC_TIMEOUT_WAITING_FOR_DCM 0x98130029: Timeout waiting for DCM ### EC_SIGNATURE_MISMATCH 0x98130030: Signature mismatch ### EC_PDIWATCHDOG 0x98130031: PDI watchdog expired ### EC_BAD_CONNECTION 0x98130032: Bad connection ### EC_XML_INCONSISTENT 0x98130033: ENI: Inconsistent content ### EC_ERROR_LAST2 EC_ERROR_LAST2. ### EMRAS_INVALIDCOOKIE 0x98110181: RAS: Invalid Cookie (e.g.obsolete) ### EMRAS_MULSRVDISMULCON 0x98110183: RAS: Connect 2nd server denied because Multi Server support is disabled (obsolete) ### EMRAS_LOGONCANCELLED 0x98110184: RAS: Logon canceled (Server-side connection reject while opening a client connection.) ### EMRAS_INVALIDVERSION 0x98110186: RAS: Invalid Version (Connection reject because of using mismatching protocol versions on client and server side) ### EMRAS_INVALIDACCESSCONFIG 0x98110187: RAS: Access configuration is invalid (e.g. SPoC access configuration invalid) ### EMRAS_ACCESSLESS 0x98110188: RAS: No access to this call at this access level (e.g. a higher SPoC access level is needed to use the called Remote API function) ### EMRAS_INVALIDDATARECEIVED 0x98110189: RAS: Invalid data received (communication corrupted) ### EMRAS_SERVERSTOPPED 0x98110191: RAS: Server stopped (e.g. connection dropped because of Remote API Server stop) ### EMRAS_WDEXPIRED 0x98110192: RAS: Watchdog expired (e.g. connection dropped because of missing keep-alive messages) ### EMRAS_RECONEXPIRED 0x98110193: RAS: Reconnect expired (obsolete) ### EMRAS_CLIENTLOGON 0x98110194: RAS Server: Client logged on ### EMRAS_RECONNECT 0x98110195: RAS: obsolete ### EMRAS_SOCKCHANGE 0x98110196: RAS: Socket exchanged after reconnect (obsolete) ### EMRAS_CLNTDISC 0x98110197: RAS: Client disconnect ### EMRAS_ACCESS_NOT_FOUND 0x98110198: RAS: Access not configured for this call (e.g. SPoC access configuration missing) ### EMRAS_TOKEN_MISSING 0x98110199: RAS: Token missing ### EMRAS_TOKEN_INVALID 0x9811019A: RAS: Token invalid ### EMRAS_TOKEN_DENIED 0x9811019B: RAS: Token denied ### EMRAS_TLS_CERTIFICATE_ERROR 0x9811019C: RAS: TLS certificate error ### EMRAS_TLS_PRIVATEKEY_ERROR 0x9811019D: RAS: TLS private key error ### EMRAS_TLS_HANDSHAKE_FAILED 0x9811019E: RAS: TLS handshake failed ### EMRAS_ERROR_LAST EMRAS_ERROR_LAST.