# Examples ## CoeSdoUpload ```csharp public void CoeSdoUploadExample() { ushort wSlaveAddress = 1012; // slave with station address 1012 ushort wObIndex = 0x1018; // object index 0x1018 byte byObSubIndex = 1; // subindex 1 (Vendor ID, which is from type UDINT with 4 bytes) uint dwDataLen = 4; // 4 bytes byte[] pbyData = new byte[dwDataLen]; uint dwOutDataLen = 0; uint dwTimeout = 5000; // timeout 5s uint dwFlags = (uint)EMailBoxFlags.NONE; // no complete access uint dwSlaveId = m_oEcWrapper.GetSlaveId(wSlaveAddress); ECError eRes = m_oEcWrapper.CoeSdoUpload(dwSlaveId, wObIndex, byObSubIndex, pbyData, dwDataLen, out dwOutDataLen, dwTimeout, dwFlags); if (eRes != ECError.EC_NOERROR) { LogMasterError("CoeSdoUpload failed: ", eRes); return; } string szValue = CEcWrapperDotNet.ConvValueToString(DN_EC_T_DEFTYPE.ARRAY_OF_BYTE, pbyData); LogInfo("CoeSdoUpload success: " + szValue); // 02 00 00 00 } ``` ## CoeSdoDownload ```csharp public void CoeSdoDownloadExample() { ushort wSlaveAddress = 1012; // slave with station address 1012 ushort wObIndex = 0x40A2; // object index 0x40A2 byte byObSubIndex = 2; // subindex 2 uint dwValue = 123; // value 123 uint dwTimeout = 5000; // timeout 5s uint dwFlags = (uint)EMailBoxFlags.NONE; // no complete access // convert UNSIGNED32 value to 4 bytes byte[] pbyData = null; ECError eRes = CEcWrapperDotNet.ConvValueToBytes(DN_EC_T_DEFTYPE.UNSIGNED32, dwValue, out pbyData); if (eRes != ECError.EC_NOERROR) { LogMasterError("ConvValueToBytes failed: ", eRes); return ; } uint dwSlaveId = m_oEcWrapper.GetSlaveId(wSlaveAddress); eRes = m_oEcWrapper.CoeSdoDownload(dwSlaveId, wObIndex, byObSubIndex, pbyData, (uint)pbyData.Length, dwTimeout, dwFlags); if (eRes != ECError.EC_NOERROR) { LogMasterError("CoeSdoDownload failed: ", eRes); return; } LogInfo("CoeSdoDownload success"); } ``` ## ReadSlaveEEPRom ```csharp public void ReadSlaveEEPRomExample() { bool bFixedAddressing = true; // enable fixed addressing ushort wSlaveAddress = 1006; // slave with station address 1006 ushort wEEPRomStartOffset = 0x0; // offset 0 uint dwReadLen = 10; // 10 bytes byte[] pwReadData = new byte[dwReadLen]; uint dwNumOutData = 0; uint dwTimeout = 2000; // timeout 2s ECError eRes = m_oEcWrapper.ReadSlaveEEPRom(bFixedAddressing, wSlaveAddress, wEEPRomStartOffset, pwReadData, dwReadLen, out dwNumOutData, dwTimeout); if (eRes != ECError.EC_NOERROR) { LogMasterError("ReadSlaveEEPRom failed: ", eRes); return; } string szValue = CEcWrapperDotNet.ConvValueToString(DN_EC_T_DEFTYPE.ARRAY_OF_BYTE, pwReadData); LogInfo("ReadSlaveEEPRom success: " + szValue); } ``` ## FoeFileDownload ```csharp public void FoeFileDownloadExample() { ushort wSlaveAddress = 1012; // slave with station address 1012 string szFileName = "foe.txt"; // filename of file in slave byte[] pbyData = new byte[] { 1, 2, 3, 4 }; // 4 bytes uint dwPassword = 0; // password is 0 uint dwTimeout = 2000; // timeout 2s uint dwSlaveId = m_oEcWrapper.GetSlaveId(wSlaveAddress); ECError eRes = m_oEcWrapper.FoeFileDownload(dwSlaveId, szFileName, (uint)szFileName.Length, pbyData, (uint)pbyData.Length, dwPassword, dwTimeout); if (eRes != ECError.EC_NOERROR) { LogMasterError("FoeFileDownload failed: ", eRes); return; } LogInfo("FoeFileDownload success"); } ```