# Introduction The .NET Wrapper provides a .NET interface to use EC-Master, EC-Monitor, EC-Simulator and RAS Client/Server. ## Requirements Microsoft .NET Framework : - Windows (x86/x64) : - Microsoft Windows 10 and above - Microsoft .NET Framework 4 Client Profile - Microsoft Visual C++ 2015 Runtime - Linux (x86/x64) : - Mono 3.2 and above (install mono-cmplete) Microsoft .NET Core : - Windows (x86/x64) : - Microsoft Windows 10 and above - Microsoft Visual C++ 2015 Runtime - Linux (x64/ARM) : - Ubuntu 18.04 and above - .NET Core 3.1 Runtime : - [https://dotnet.microsoft.com/en-us/download/dotnet](https://dotnet.microsoft.com/en-us/download/dotnet) ## Architecture ![.NET programming interface layer model](Media/architecture.svg) The architecture contains 4 basic layers: Customer .NET application or our examples (EcMasterDemoDotNet, …) : - Demo application, written in C# Programming Interface (EcWrapperDotNet) : - Provides an object oriented API written in .NET Wrapper Library (EcWrapper) : - Native wrapper library, which provides API for object oriented access Native Libraries : - EC-Master Library - EC-Monitor LIbrary - EC-Simulator Library - RAS Client Library