# FAQ PyQt5 cannot be installed on Ubuntu 14.04 x64, because it requires Python 3.5. How can I install it? > It can be installed by calling > ```console > $ sudo apt-get install python3-pyqt5 > ``` I installed Python and the demo crashes with strange errors. What can I do? > This might be a problem of mixing x86 with x64 binaries. Verify that if you have installed the Python runtime for x64 bit, please install also EC-Master for x64 bit.