# emllDpdk
Linux® DPDK. Hardware independent network driver.
#### SEE ALSO
[User Manual](../ec-master-class-b/emlldpdk.html)
## Supported OS and Arch
| | Linux |
|---------------------------|---------------------------------------|
| Architecture | ARM_64
x86_64
|
| Interrupt
supported | ❌ |
| Fingerprint
supported | ❌ |
## Supported NICs
The following reference Network Interface Cards have been successfully tested.
- NXP Layerscape 1046A
- NXP i.MX95
- Intel Ethernet Network Adapter X710
- Intel Ethernet-Controller I210
The complete list of NICs supported by DPDK is available at [https://core.dpdk.org/supported/nics/](https://core.dpdk.org/supported/nics/)