7.1. Link Layer selection
The EC-Monitor currently supports a variety of different Link Layer modules, each of which contained in a single library file, which is loaded by the core library dynamically. The EC-Monitor shipment consist of a core library and one (or more) libraries each containing support for one specific Link Layer module (type of hardware card). Which library actually is loaded, is depending on the Link Layer parameters at runtime.
The principle of Link Layer selection is that the name of the Link Layer (Link Layer Identification) is used to determine the location and name of a registration function, which is called by the EC-Monitor and registers function pointers which allow access to the Link Layer functional entries.
The EtherCAT Link Layer will be initialized using a Link Layer specific configuration parameter set. A pointer to this parameter set is part of the EC-Monitor initialization settings.
The EC-Monitor supports two Link Layer operating modes. If the Link Layer operates in interrupt mode all received Ethernet frames will be processed immediately in the context of the Link Layer receiver task. When using the polling mode the EC-Monitor will call the Link Layer receiver polling function prior to processing received frames.
7.1.1. Optimized Link Layer drivers
Optimized means operating directly on the network device’s register set instead of using the operating system’s native driver.
7.1.2. Optimized Link Layer drivers and PHY OS Driver
Some operating systems, e.g. Linux and Xenomai, provide drivers for most common Ethernet controllers and their related physical transceivers (PHY). The manufacturer specific PHY circuits can be handled by a dedicated driver. Using the PHY OS Driver interface it is possible to use the manufacturer’s dedicated PHY driver without modification of the acontis optimized Link Layer driver. Depending on the hardware architecture, an additional module from acontis, e.g. atemsys for Linux, grants access to the MDIO bus to the OS drivers, or request MDIO operations from the OS drivers.
Note
Link Layer modules not listed here may be available if purchased additionally
7.1.3. Link Layer selection and initialization
The different Link Layer modules are selected and parameterized by a common structure EC_T_LINK_PARMS
shared by all Link Layers and a Link Layer specific structure, pointed to by an element within the common structure. This parameter set is given to EC_T_INIT_MONITOR_PARMS::pLinkParms
with the call of emInitMonitor()
.
-
struct EC_T_LINK_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Signature of the adapter specific structure containing the EC_T_LINK_PARMS structure
-
EC_T_DWORD dwSize
[in] Size of the adapter specific structure containing the EC_T_LINK_PARMS structure
-
EC_T_LOG_PARMS LogParms
[in] Logging parameters
-
EC_T_CHAR szDriverIdent[EC_DRIVER_IDENT_NAMESIZE]
[in] Name of Link Layer module (driver identification) for Link Layer Selection
-
EC_T_DWORD dwInstance
[in] Instance of the adapter. if EC_LINKUNIT_PCILOCATION is set: contains PCI address
-
EC_T_DWORD dwIstPriority
[in] Task priority of the interrupt service task (not used in polling mode)
-
EC_T_DWORD dwSignature
-
struct EC_T_LINK_TTS
Public Members
-
EC_T_BOOL bEnabled
[in] Use Time-Triggered Send
-
EC_T_DWORD dwCycleTimeUsec
[in] Cycle time between 2 pfnStartCycle calls
-
EC_T_DWORD dwSendOffsetUsec
[in] Time between pfnStartCycle call and frame transmission
-
EC_T_BOOL bEnabled
7.1.4. Link Layer instance selection via PCI location
For some operating systems it is possible to address the Link Layer instance using its PCI address as an alternative. To do this, EC_LINKUNIT_PCILOCATION (0x01000000) and the PCI location must be set as EC_T_LINK_PARMS::dwInstance
.
On Linux the PCI address can be shown using e.g.:
lspci | grep Ethernet
00:19.0 Ethernet controller: Intel Corporation Ethernet Connection I217-LM (rev 04)
04:00.0 Ethernet controller: Intel Corporation 82574L Gigabit Network Connection
05:00.0 Ethernet controller: Intel Corporation 82574L Gigabit Network Connection
The format of EC_T_LINK_PARMS::dwInstance
using PCI bus address is:
- 0x01bbddff
bb Bus Number
dd Device Number
ff Function Number
EC_T_LINK_PARMS::dwInstance = 0x01001900; //"0000:00:19.0"
On Windows the integer value displayed in properties dialog must be converted to HEX. E.g the number from the following dialog (PCI bus 11, device 0, function 0) corresponds to 0x010B0000 (bus 0x0B).