# Application programming interface, reference Function prototypes, definitions etc. of the API can be found in the header file `EcMonitor.h` which is the main header file to include when using EC-Monitor. ### Fundamental types ### typedef void \*EC_T_PVOID Pointer of type void ### typedef int EC_T_BOOL Boolean ### typedef char EC_T_CHAR Character, 8 bit ### typedef unsigned short EC_T_WCHAR Wide-character, 16 bit ### typedef unsigned char EC_T_BYTE Byte, unsigned integer 8 bit ### typedef unsigned char \*EC_T_PBYTE Pointer of type EC_T_BYTE ### typedef unsigned short EC_T_WORD Word, unsigned integer 16 bit ### typedef unsigned int EC_T_DWORD Double word, unsigned integer 32 bit ### typedef signed char EC_T_SBYTE Signed-Byte, signed integer 8 bit ### typedef signed short EC_T_SWORD Signed-Word, signed integer 16 bit ### typedef signed int EC_T_SDWORD Signed-Double-Word, signed integer 32 bit ### typedef int EC_T_INT Integer ### typedef unsigned int EC_T_UINT Unsigned-Integer ### typedef short EC_T_SHORT Short ### typedef unsigned short EC_T_USHORT Unsigned-Short ### typedef float EC_T_REAL Real, floating point ### typedef double EC_T_LREAL long Real, floating point ### typedef unsigned long long EC_T_UINT64 Unsigned integer 64 bits ### typedef signed long long EC_T_INT64 Signed integer 64 bits ### EC_T_VOID Void type ### Macros ### EC_TRUE Boolean value: True ### EC_FALSE Boolean value: False ### EC_NULL Null pointer constant