# Windows TAP - emllTap The parameters to the Windows TAP Real-time Ethernet Driver are setup-specific. The function `CreateLinkParmsFromCmdLineTap()` in [`EcSelectLinkLayer.cpp`](_downloads/bf62c71a4a7e317930818b9da4a9815c/EcSelectLinkLayer.cpp) demonstrates how to initialize the Real-time Ethernet Driver instance. ### struct EC_T_LINK_PARMS_TAP ### Public Members ### [EC_T_LINK_PARMS](emll_generic.html.md#_CPPv415EC_T_LINK_PARMS) linkParms Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_TAP. ### [EC_T_CHAR](api.html.md#_CPPv49EC_T_CHAR) szAdapterName[EC_TAP_ADAPTER_NAME_SIZE] Native tap device name, e.g. “tap0” (zero terminated) ### [EC_T_CHAR](api.html.md#_CPPv49EC_T_CHAR) szAdapterGuid[EC_TAP_ADAPTER_GUID_SIZE] GUID of virtual interface to connect (zero terminated) ### [EC_T_BYTE](api.html.md#_CPPv49EC_T_BYTE) abyMac[6] MAC address ### [EC_T_DWORD](api.html.md#_CPPv410EC_T_DWORD) dwRxBufferCnt Frame buffer count for IST The adapter must be manually installed as described in the OpenVPN’s Windows TAP-driver manual, see [https://community.openvpn.net/openvpn/wiki/GettingTapWindows](https://community.openvpn.net/openvpn/wiki/GettingTapWindows) . While EC-Monitor is connected to the adapter using emllTap, the MainDevice can use it with e.g. emllNdis.