# EtherCAT® Network Configuration ENI The EtherCAT® configuration file ENI contains one or more Cyclic entries for reading new input data values and output data values (process data update). These entries contain one or more frames, so-called cyclic frames, which are to be sent cyclically by the EtherCAT® MainDevice. Within the cyclic frames are one or more EtherCAT® datagrams that contain logical read/write commands for accessing the process data values. ## Single cyclic entry configuration In the simplest case, there is only a single cyclic entry with one or more cyclic frames. ![Diagram of a single cyclic entry ENI configuration with one or more cyclic frames containing EtherCAT datagrams for process data updates](../Media/Eni_SingleCycEntry.png) ## Multiple cyclic entries configuration For more complex scenarios it is possible to configure the system using multiple cyclic entries with one or more cyclic frames for each cyclic entry. ![Diagram of a multiple cyclic entries ENI configuration with separate sets of cyclic frames for each cyclic entry](../Media/Eni_MultipleCycEntry.png)