# Platform and Operating Systems (OS) EC-Monitor and the EcMonitorDemo example application support a range of operating systems and platforms. This chapter covers OS-specific setup, build, and compiler settings for each supported platform. EC-Monitor is implemented in portable C++ and contains no direct operating system call. Everything it requires from its environment, such as memory, threads, synchronization and time, is obtained through a small OS layer. Only this layer is platform dependent, all other sources are built unmodified on every supported platform. The OS layer interface is declared in the header file `EcOs.h` and covers the following services: Memory : Allocation as well as memory and string operations. Threads : Thread creation including priority and CPU affinity. Synchronization : Locks of several types and events. Time : Millisecond tick, sleep, host system time and high resolution counter. Module loading : Binding of the [Real-time Ethernet Driver](emll.html.md#real-time-ethernet-driver) at runtime on platforms supporting dynamically loaded modules. Debug : Assertions and string formatting. The platform specific implementation consists of `EcOsPlatform.h` and `EcOs.cpp`. Most functions are that easy that they can be implemented using simple C macros mapping to the native API. Implementations for all platforms listed below are part of a source code delivery, see [source code delivery](integration_src.html.md#product-source-code). The OS layer is initialized with `EC_T_OS_PARMS`, either by calling `OsInit()` as done by the demo applications, or by [`EC_T_MONITOR_INIT_PARMS::pOsParms`](api_general.html.md#_CPPv4N23EC_T_MONITOR_INIT_PARMS8pOsParmsE) when calling [`emonInitMonitor()`](api_general.html.md#_CPPv415emonInitMonitor10EC_T_DWORDPK23EC_T_MONITOR_INIT_PARMS). #### NOTE Real-time behaviour is determined by the operating system and not by EC-Monitor.