# INtime HPE - emllHPE emllHPE is part of EC-Simulator for INtime. emllHPE uses the INtime High-Performance Ethernet (HPE) interface. The parameters to emllHPE are setup-specific. The function `CreateLinkParmsFromCmdLineHPE()` in [`EcSelectLinkLayer.cpp`](_downloads/bf62c71a4a7e317930818b9da4a9815c/EcSelectLinkLayer.cpp) demonstrates how to initialize the Real-time Ethernet Driver instance. ### struct EC_T_LINK_PARMS_HPE ### Public Members ### [EC_T_LINK_PARMS](emll_init.html.md#_CPPv415EC_T_LINK_PARMS) linkParms Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_HPE. ### [EC_T_CHAR](api.html.md#_CPPv49EC_T_CHAR) szAdapterName[EC_HPE_ADAPTER_NAME_SIZE] Name of Ethernet Interface, e.g. “ie1g0” ### [EC_T_DWORD](api.html.md#_CPPv410EC_T_DWORD) dwRxBufferCnt Receive buffer count ### [EC_T_DWORD](api.html.md#_CPPv410EC_T_DWORD) dwTxBufferCnt Transmit buffer count ### [EC_T_BOOL](api.html.md#_CPPv49EC_T_BOOL) bDisableForceBroadcast Don’t change target MAC address to FF:FF:FF:FF:FF:FF