# Error Codes
### Groups
| **No.** | **Group** | **Abbr.** | **Description** |
|-----------|--------------------------------------------|-------------|----------------------------------------------------------------------------------------------------------------|
| 1 | Application Error | APP | Error within application, running the Simulator
E.g. API function call with invalid parameters |
| 2 | EtherCAT® network information file problem | ENI | Network configuration XML file error
E.g. malformed or empty EtherCAT® Network configuration file |
| 3 | Simulator parameter configuration | CFG | Simulator configuration parameters erroneous
E.g. mailbox command queue not large enough |
| 4 | Bus/SubDevice Error | SLV | SubDevice error
E.g. Working Counter Error |
| 5 | Real-time Ethernet Driver | LLA | Real-time Ethernet Driver error (network interface driver)
E.g. Intel Pro/1000 NIC could not be found |
| 6 | Remote API | RAS | Remote API error
E.g. connection to Remote API server is not possible from client |
| 7 | Internal software error | ISW | Simulator internal error |