# EC-Simulator Python

> EC-Simulator Python documentation


2026-Oct-14, acontis technologies GmbH

## Pages

- [Python Programming Interface](index.html.md): Main documentation page
- [Introduction](introduction.html.md): The Python Wrapper provides a Python interface to use EC-Master, EC-Monitor, EC-Simulator and RAS Cl...
- [Programmers Guide](programmers-guide.html.md): This chapter walks through the sample scripts and sample code shipped with the wrapper, describes th...
- [Sample Scripts](programmers-guide_sample-scripts.html.md): There are currently 2 scripts available:
- [Sample Code](programmers-guide_sample-code.html.md): The Python demo application contains of 3 modules:
- [Wrapper](programmers-guide_wrapper.html.md): The Python Wrapper contains of 5 modules:
- [Supported IDEs](programmers-guide_supported-ides.html.md): This is the default IDE.
- [Application programming interface, reference](api.html.md): Function prototypes, definitions etc. of the API can be found in `EcWrapperPython.py` and `EcWrapper...
- [Examples](examples.html.md): def CoeSdoUploadExample(self):
- [FAQ](faq.html.md): PyQt5 cannot be installed on Ubuntu 14.04 x64, because it requires Python 3.5. How can I install it?

---

For more comprehensive documentation, see [llms-full.txt](llms-full.txt)