2. Programmers Guide

2.1. Sample Scripts

There are currently 2 scripts available:

EcMasterDemoPython.bat

Starts the console demo application

EcMasterDemoPythonInteractive.bat

Starts the interactive demo application

The scripts will start the demo application. The interactive demo application waits for user input where the user can enter the following commands:

# Write variable
demo.processImage.variables.Slave_1005__EL2008_.Channel_1.Output.set(1)

# Read variable
demo.processImage.variables.Slave_1005__EL2008_.Channel_1.Output.get()

# Print properties of variable
demo.processImage.variables.Slave_1005__EL2008_.Channel_1.Output.dmp()

# Stop the demo:
demo.stopDemo()

2.2. Sample Code

The Python demo application contains of 3 modules:

EcDemoApp.py:

Console demo application

EcDemoAppGui.py:

Gui demo application, based on Qt5

EcDemoAppInteractive.py:

Interactive demo application

2.3. Wrapper

2.3.1. Modules

The Python Wrapper contains of 5 modules:

EcWrapperPython.py
class CEcWrapperPython

EC-Wrapper base class

class CEcMasterPython

EC-Master

class CEcMasterRasServerPython

RAS Server for EC-Master

class CEcMasterMbxGatewayClientPython

Mailbox Gateway Client for EC-Master

class CEcMasterMbxGatewayServerPython

Mailbox Gateway Server for EC-Master

class CEcSimulatorPython

EC-Simulator

class CEcSimulatorRasServerPython

RAS Server for EC-Simulator

class CEcRasClientPython

RAS Client for EC-Master / EC-Simulator

EcMotionPython.py
class CEcMotionPython

EC-Motion interface

EcWrapperPythonTypes.py

Python types

EcWrapper.py

CPython interface (internal)

EcWrapperTypes.py

CPython types (internal)

2.3.2. Return code vs. exception handling

The most of all API functions returns a return code for error handling. This behaviour can be changed to throw an exception in error case by simply setting:

CEcWrapperPython.EnableExceptionHandling = True # default is False

2.3.3. API with “out” or “ref” parameters

The Python Wrapper API is based on C# code. C# supports out and ref keywords for parameters. This is not supported in Python and is solved by simply submitting CEcWrapperPythonOutParam or CEcWrapperPythonRefParam to those functions:

# This function has an "out" parameter "out_oSbStatus"
def GetScanBusStatus(self, out_oSbStatus):
    # ...
    return

# Create "out" parameter
out_oStatus = CEcWrapperPythonOutParam()
# Call function
pythonWrapper.GetScanBusStatus(out_oStatus)
# Get the "out" parameter value
oStatus = out_oStatus.value
# Now, the "oStatus" object can be used
print(oStatus.dwResultCode)

2.4. Supported IDEs

2.4.1. Python Shell IDLE

This is the default IDE.

It can be started from Windows Start Menu or by calling C:/Python/Lib/idlelib/idle.py:
Python IDLE shell window showing the default IDE environment for running Python code
In this shell, the user can simply copy&paste the sample code from: Examples/EcMasterDemoPython/EcDemoAppInteractive.py
exec("""
import os
import sys
INSTALLDIR = "C:/Program
Files/acontis_technologies/EC-Master-Windows-x86_64Bit/"
os.environ["PATH"] += os.pathsep + INSTALLDIR + "Bin/Windows/x64"
sys.path.append(INSTALLDIR + "Sources/EcWrapperPython")
sys.path.append(INSTALLDIR + "Examples/EcMasterDemoPython")
from EcDemoApp import \*
demo = EcMasterDemoPython()
demo.pAppParms.tRunMode = RunMode.Master
demo.pAppParms.dwBusCycleTimeUsec = 4000
demo.pAppParms.szENIFilename = "ENI.xml"
demo.pAppParms.szLinkLayer = "ndis 127.0.0.0 1"
demo.pAppParms.nVerbose = 3
demo.startDemo()
print("EcMasterDemoPython is running.")
print("Type demo.help() for interactive help.")
""")
… and the demo is running.
Python IDLE shell window showing EcMasterDemoPython running in interactive mode

2.4.2. Visual Studio 2019

Create a new project:
Visual Studio 2019 shows create a new project dialog
Configure the project:
  • Replace the generated file EcMasterDemoPython.py with the existing EcDemoApp.py.

Visual Studio 2019 shows configure your new project dialog
Configure project General settings:
  • Startup File: EcDemoApp.py

Visual Studio 2019 shows general tab of new generated Python appliation project
Configure project Debug settings:
  • Search Paths:

../../Sources/EcWrapperPython;../EcMasterDemoPython
  • Script Arguments:

-mode 1 -file ENI.xml -link "ndis 127.0.0.0 1 1" -cycletime 4000 -time 1000 -lvl 3
  • Environment Variables:

PATH=../../Bin/Windows/x64;%PATH%
Visual Studio 2019 shows debug tab of new generated Python appliation project
Press Start and the demo is running:
Command prompt window showing EcMasterDemoPython

2.4.3. Visual Studio Code

Install python extension by open extension tab and enter python:
Visual Studio Code Extensions tab showing the Python extension
Open folder Examples/EcMasterDemoPython and configure the launch.json:
{
    "version": "0.2.0",
    "configurations": [
        {
            "name": "Python: Aktuelle Datei",
            "type": "python",
            "request": "launch",
            "program": "${file}",
            "console": "integratedTerminal",
            "cwd": "",
            "args" : [
                "-mode", "1",
                "-file", "ENI.xml",
                "-link", "ndis 127.0.0.1 1",
                "-cycleTime", "4000",
                "-time", "1000",
                "-lvl", "3",
            ],
            "env": {"PYTHONPATH": "${workspaceRoot}"}
        }
    ]
}
Visual Studio Code showing the launch.json configuration for running EcMasterDemoPython with cmdline parameters
Configure linter in settings.json:
{
      "git.ignoreLimitWarning": true,
      "python.linting.pylintArgs": [
          "--init-hook='import sys; sys.path.append(\"C:/Temp/EC-Master-Windows-x86_64Bit/Sources/EcWrapperPython\")'"
      ]
}
Visual Studio Code showing the settings.json configuration for Python linter
Open EcDemoApp.py and the following lines to set environment:
import os
import sys
INSTALLDIR = "C:/Temp/EC-Master-Windows-x86_64Bit/"
os.environ["PATH"] += os.pathsep + INSTALLDIR + "Bin/Windows/x64"
sys.path.append(INSTALLDIR + "Sources/EcWrapperPython")
sys.path.append(INSTALLDIR + "Examples/EcMasterDemoPython")
Visual Studio Code showing EcDemoApp.py with possbile environment setup lines
Start debugging and the demo output will be written into the terminal:
Visual Studio Code debug session showing EcMasterDemoPython console output in the integrated terminal