# Sample Scripts There are currently 2 scripts available: `EcMasterDemoPython.bat` : Starts the console demo application `EcMasterDemoPythonInteractive.bat` : Starts the interactive demo application The scripts will start the demo application. The interactive demo application waits for user input where the user can enter the following commands: ```python # Write variable demo.processImage.variables.Slave_1005__EL2008_.Channel_1.Output.set(1) # Read variable demo.processImage.variables.Slave_1005__EL2008_.Channel_1.Output.get() # Print properties of variable demo.processImage.variables.Slave_1005__EL2008_.Channel_1.Output.dmp() # Stop the demo: demo.stopDemo() ```