# Broadcom NetXtreme - emllBcmNetXtreme The parameters to the Real-time Ethernet Driver Broadcom® NetXtreme are setup-specific. The function `CreateLinkParmsFromCmdLineBcmNetXtreme()` in [`EcSelectLinkLayer.cpp`](_downloads/bf62c71a4a7e317930818b9da4a9815c/EcSelectLinkLayer.cpp) demonstrates how to initialize the Link Layer instance. ### struct EC_T_LINK_PARMS_BCMNETXTREME ### Public Members ### [EC_T_LINK_PARMS](emll_init.html.md#_CPPv415EC_T_LINK_PARMS) linkParms Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_BCMNETXTREME. ### [EC_T_DWORD](api.html.md#_CPPv410EC_T_DWORD) dwRxBuffers Receive buffer count. Must be a power of 2, maximum 1024. ### [EC_T_DWORD](api.html.md#_CPPv410EC_T_DWORD) dwTxBuffers Transmit buffer count. Must be a power of 2, maximum 1024. ## Supported PCI devices Broadcom 571x PCI specific definitions (VendorId, DeviceId)