# Texas Instruments ICSS - emllICSS The parameters to the Real-time Ethernet Driver ICSS are setup-specific. The function `CreateLinkParmsFromCmdLineICSS()` in [`EcSelectLinkLayer.cpp`](_downloads/bf62c71a4a7e317930818b9da4a9815c/EcSelectLinkLayer.cpp) demonstrates how to initialize the Real-time Ethernet Driver instance. ### struct EC_T_LINK_PARMS_ICSS ### Public Members ### [EC_T_LINK_PARMS](emll_init.html.md#_CPPv415EC_T_LINK_PARMS) linkParms Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_ICSS. ### [EC_T_LINK_ICSS_BOARD](#_CPPv420EC_T_LINK_ICSS_BOARD) eBoardType TI System on Chip board type ### [EC_T_BOOL](api.html.md#_CPPv49EC_T_BOOL) bMaster Initialize whole PRUSS subsystem, not only port. This flag is always required when the link layer is used on a single ICSS port. This flag is also required, when the link layer is used in “Redundancy mode” and two ICSS ports are used. In this case, first port should be master, and second port should be slave. ### [EC_T_BOOL](api.html.md#_CPPv49EC_T_BOOL) bNoMacAddr EC_TRUE: No MAC address registers access ### [EC_T_DWORD](api.html.md#_CPPv410EC_T_DWORD) dwPhyAddr PHY address ### [EC_T_PHYINTERFACE](emll_init.html.md#_CPPv417EC_T_PHYINTERFACE) ePhyInterface PHY connection type ### [EC_T_BOOL](api.html.md#_CPPv49EC_T_BOOL) bNoPhyReset No hardware reset of the PHY ### [EC_T_BOOL](api.html.md#_CPPv49EC_T_BOOL) bUseAllSendQueues Use the additional 3 queues with lower priority to send more frames per cycle ### [EC_T_BOOL](api.html.md#_CPPv49EC_T_BOOL) bLegacyFirmware For am57xx use legacy ICSS firmware from pdk_am57xx_1_0_6, instead of pdk_am57xx_1_0_17 with patch for Rx error issue, see [https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1022410/am5746-rx_error_offset-conditions/3788558#3788558](https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1022410/am5746-rx_error_offset-conditions/3788558#3788558) ### enum EC_T_LINK_ICSS_BOARD *Values:* ### enumerator EcLinkIcssBoard_Unsupported ### enumerator EcLinkIcssBoard_am572x TI AM572x ### enumerator EcLinkIcssBoard_am571x TI AM571x ### enumerator EcLinkIcssBoard_am3359 TI AM3359 ### enumerator EcLinkIcssBoard_am572x_emerson TI AM572x on Emerson board ### enumerator EcLinkIcssBoard_am574x TI AM574x ## TTS Feature Real-time Ethernet Driver PRU ICSS can optionally use Time-Triggered Send feature [https://www.ti.com/lit/pdf/tidubz1](https://www.ti.com/lit/pdf/tidubz1) To test it, you need to build a demo application with INCLUDE_TTS macro. Additionally, you need to set the bTts flag and configure other tts parameters in [`EC_T_LINK_PARMS_ICSS`](#_CPPv420EC_T_LINK_PARMS_ICSS) structure. Please note, we have already TTS Demo applications for some of the operating systems (for ex. Linux and TI RTOS). dwTtsSendTimeUsec time is determined experimentally. It depends on how long your own real project prepares cyclic and acyclic frames to be sent in the current cycle. The main purpose of the TTS feature is to reduce jitter to 40 ns (nanoseconds). To measure jitter accurately you need to have special software and hardware. For example: - Old version of Wire Shark, ex. 1.8.4 - Dissect plugin for Wire Shark (this plugin is available only for this version of WireShark) - ET2000 device to insert accurate timestamps with nanoseconds resolution. Details can be found here: [https://infosys.beckhoff.com/index.php?content=../content/1031/et2000/1309654283.html&id=](https://infosys.beckhoff.com/index.php?content=../content/1031/et2000/1309654283.html&id=) ## TI AM335x ICEV2 After the two 100 MBit ports have been deactivated, there are no longer any Ethernet ports that can be used for TCP/IP. The board cannot work in mixed mode, i.e. there is no CPSW+ICSS support. It is also necessary to configure the board to start in ICSS rather than CPSW mode. Set both jumpers on the board to ICSS mode. #### SEE ALSO [http://processors.wiki.ti.com/index.php/AM335x_Industrial_Communication_Engine_EVM_Rev2_1_HW_User_Guide](http://processors.wiki.ti.com/index.php/AM335x_Industrial_Communication_Engine_EVM_Rev2_1_HW_User_Guide) ## TI AM57xx IDK After the four 100 MBit ports of the ICSS have been deactivated, the other two 1 GBit ports (CPSW) remain active and can be used for other purposes (e.g. TCP / IP). ## AM5728 IDK and AM5718 IDK boards and Technical Limitations The main difference between these two boards is number of available ICSS ports. AM5728 IDK supports only two 100 Mbit ports: port 3 and 4. It is a technical limitation of this board. On AM5718 IDK all four 100 Mbit ports are available for EtherCAT® purposes. #### NOTE Real-time Ethernet Driver PRUICSS can use at most 2 ports together (in redundancy mode) and these two ports should correspond to the same PRUSS. I.e. Port 3 and 4 OR Port 1 and 2, but not Port 1 and 4, Port 1 and 3 and etc. This technical limitation exists, because PRU firmware for PRU0 and PRU1 uses the same memory areas of OCMC Memory. In the future, this limitation can be removed.