# Error Codes ### Groups | **No.** | **Group** | **Abbr.** | **Description** | |-----------|--------------------------------------------|-------------|----------------------------------------------------------------------------------------------------------------| | 1 | Application Error | APP | Error within application, running the Simulator

E.g. API function call with invalid parameters | | 2 | EtherCAT® network information file problem | ENI | Network configuration XML file error

E.g. malformed or empty EtherCAT® Network configuration file | | 3 | Simulator parameter configuration | CFG | Simulator configuration parameters erroneous

E.g. mailbox command queue not large enough | | 4 | Bus/SubDevice Error | SLV | SubDevice error

E.g. Working Counter Error | | 5 | Real-time Ethernet Driver | LLA | Real-time Ethernet Driver error (network interface driver)

E.g. Intel Pro/1000 NIC could not be found | | 6 | Remote API | RAS | Remote API error

E.g. connection to Remote API server is not possible from client | | 7 | Internal software error | ISW | Simulator internal error |