# tenAsys INtime Real-time Ethernet Drivers are available for INtime. If using INtime with Windows running in parallel on the same host the network adapter has to be assigned to INtime. The network adapters should be passed to INtime using the `INtime Device Manager`. Please refer to the INtime user manual for this. Search locations for Real-time Ethernet Drivers can be adjusted using the `PATH` environment variable. ## OS Compiler settings Besides the general settings from [OS Compiler settings](architecture_sdk.html.md#compile-ecdemo) the following settings are necessary to build the example application for INtime. Extra include paths : ```default \SDK\INC\INtime \Examples\Common\INtime ``` Extra source paths : ```default \Examples\Common\INtime \Sources\OsLayer\INtime ``` Extra library paths to the main EtherCAT® components : ```default \SDK\LIB\INtime ```