\\newpage # IntervalZero RTX EC-Simulator HiL is available for RTX64 3.x and RTX64 4.x . ## OS Compiler settings Besides the general settings from [OS Compiler settings](architecture_sdk.html.md#compile-ecdemo) the following settings are necessary to build the example application for RTX. Extra include paths : ```default \SDK\INC\RTX \Examples\Common\RTX ``` Extra source paths : ```default \Examples\Common\RTX \Sources\OsLayer\RTX ``` Extra library paths to the main EtherCAT® components : ```default \SDK\LIB\RTX64 (RTX64 4.x) \SDK\LIB\RTX64_30 (RTX64 3.x) ```