1. Manual CAT Optimization
1.1. Default configuration
By default CAT is configured to be shared equally across all operating systems. The cache architecture (which cores are sharing which cache) is taken into account.
For example an x5-E3940 with 4 cores and 2 separated L2 caches:
L2-1 is shared between core index 0 and 1
L2-2 is shared between core index 2 and 3.
The architecture is coded into CPU-ID information (see Intel Software Developer Manual, Volume 2, assembler directive ‘cpuid’ for details). For analysis reports RtosUpload can display such information using:
RtosUpload.exe -nosleep -nowait -idshow 29,0,1
RtosUpload.exe -nosleep -nowait -idshow 29,0,3
(The exact idshow value might change without notice but using 0,0,0 gives a hint where to start, so does 29,0,0)
Automatic configuration examples (since 8.0.01.03)
CPU- MASK
Host RTOS Caches
0x01 0x0E L2-1 is shared 50%; L2-2 is not shared
0x03 0x0C L2-1 and L2-2 are not shared
0x07 0x08 L2-1 is not shared; L2-2 is shared 50%
1.2. Manual configuration
In “RtosVM-UserManual.pdf” chapter “CAT Config-File settings” describes how to manually configure CAT. This is an example to modify the previous example (CPU masks 0x07 and 0x08) to assign 3/4 of L2-2 to RTOS:
[Vmf\RDT]
"CatMaskL2Cos0Cpu2"=dword:C0
"CatMaskL2Cos1Cpu2"=dword:3F
Hint
The higher bits should be used for the lower prio OS because they might be shared with an onboard GPU.
1.3. Optimization
It is possible to measure the effects of CAT using the processor performance counters to measure the L1/L2/L3 cache miss. This can be used to optimize the cache allocation mask.
An example of how to measure this is included into our RTOS-32 RealtimeDemo. The demo has to be recompiled with RTMEASURE_PMC being defined.
Of course the CPU needs to support performance-counters and the used IDs.
Concept:
Configuration
- Disable all performance-counter (PMC) at MSR IA32_PERF_GLOBAL_CTRL
- Configure counter x at MSR IA32_PERFEVTSEL0, Reset counter x at MSR IA32_PMC0
- Configure counter x+1 at MSR IA32_PERFEVTSEL0+1, Reset counter x+1 at MSR IA32_PMC0+1
...
- Enable configured PMC at MSR IA32_PERF_GLOBAL_CTRL
Read counter
- Read PMC(X) using intrinsic ``__readpmc(x)`` ASM ``RDPMC``
1.4. Counters
In our RealtimeDemo the event_selector for L1-miss is 0x00000000004308D1 which will be written to MSR IA32_PERFEVTSEL0.
According to chapter “19.2.1.1 Architectural Performance Monitoring Version 1 Facilities” in SDM this means:
EN = 1 // Enable counters
OS = 1 // Count at priviledge level 0
USR = 1 // Count at priviledge level 1,2,3
Unit Mask = 0x08 // UMask=08H
Event Select = 0xD1 // EventSel=D1H
“Unit Mask” and “Event Select” can be found on https://perfmon-events.intel.com/ (EventSel=D1H UMask=08H). The event name is “MEM_LOAD_RETIRED.L1_MISS”. Modifying those values allows measuring any of the events supported by the CPU.