1. Getting Started - step-by-step tutorial¶
This manual will guide you through the following steps:
Hardware/Software setup including the Intel PRO/1000 network adapter, several EtherCAT slaves. (See Chapter Prerequisites)
Scan the EtherCAT network and configure the network.
Bring the network into operational mode.
Hint
sudo equals Windows run as administrator.
Hint
sudo -s switches user to root (administrator).
1.1. Prerequisites¶
PC/IPC with at least 1 networt device.
CPU: at least 2 cores. Default configuration is optimized for 4 cores.
HDD: at least 10GB. Additional 50GB in case of Windows-VM-Guest
preferably 1x
Intel PRO/1000(likeI210), as the scripts are preconfigured to this network adapter.
1 EtherCAT slaves to attach to the network adapter
Caution
The PC/IPC will be used to install/co-install an UBUNTU derivate!
BIOS settings
USB Legacy mode has to be disabled
Hyper-Threading shall be disabled
Power saving settings have to disabled (C-States, Speedstepping, …)