8. Additional Tools

8.1. ESI-Manager

ESI-Manager can be found through the main menu File -> ESI-Manager.

This dialog helps the user to administrate his ESI and SCI files. Here, he can add/delete/export ESI and SCI files.
../_images/esi-manager.png

8.2. EMI-Manager

EMI-Manager can be found through the main menu File -> EMI-Manager.

This dialog helps the user to administrate his EtherCAT MainDevice Information (EMI) files.
../_images/emi-manager.png

EMI files, are files which are specify the MainDevice features. Means that options and dialogs can be restricted to those features which are supported by the control system, e.g. available cycle times, support of scan for MDP modules or DC synchronization.

8.2.1. Administration

This dialog helps the user to administrate his EtherCAT MainDevice Information (EMI) files.

By default EC-EngineerWeb has two files included (read-only):

EtherCATMaster_ClassA.emi: EMI template which is prepared for configuring a “Class A” MainDevice EtherCATMaster_ClassB.emi: EMI template which is prepared for configuring a “Class B” MainDevice

If the user wants to customize EC-EngineerWeb, he can create a new EMI file with defaults, copy an existing EMI template or import an EMI file.

If he wants to add new properties to a group, he can add this only to the group “Parameters”. This group is by default empty, but if user has added some properties, he will see the list of properties on tab “Advanced Options” of the MainDevice, where the values can be modified.

../_images/master-advanced.png

8.2.2. Supported Entries

The following EMI entries are supported:

MainDevice Group
../_images/master-settings.png
Display Group:

Shows or hides group

Lock Group:

Locks or unlocks group

Name of MainDevice:

Default MainDevice name

Show name of MainDevice:

Enable if user should be able to view and change the name of the MainDevice

Lock name of MainDevice:

Enable if user should not be able to change the name of the MainDevice

Cycle Time:

Default Cycle Time

Show Cycle Time:

Enable if user should be able to view and change the Cycle Time

Lock Cycle Time:

Enable if user should not be able to change the Cycle Time

List values of Cycle Time:

Enter possible values of Cycle Time

Frequency:

Default Frequency

Show Frequency:

Enable if user should be able to view and change the Frequency

Lock Frequency:

Enable if user should not be able to change the Frequency

List values of Frequency:

Enter possible values of Frequency

Cycle Time Mode:

Enter Cycle Time Mode (0 = Cycle Time, 1 = Frequency)

Init Command Retries:

Init Command Retries

Maximal SubDevice Count:

Enter maximal count of SubDevices which are allowed to configure (0 = use default limit of MainDevice)

SubDevice Start Address:

Enter default start address for all SubDevices

Scan for MDP SubDevices:

Enable for activating MDP-Scan if it is supported from SubDevice

PDO Upload:

Enable for activating PDO upload during scan if it is supported from SubDevice

Byte-Align Process Data Image:

Enable if process data image should be byte aligned and not as small as possible

Edit Complete Variable Name:

Enable if user should be able to edit the complete variable name

Process Image Layout:

Enter process image layout features (0 = default, 0x1 = with protocol data, 0x2 = with VLAN tag, 0x4 = without frame alignment, 0x8 = alphabetic port order, 0x10 = Compatibility to ENI spec V1.0.0, 0x20 = Moves AL Status command to the end, 0x40 = Disable command splitting, 0x80 = Compatibility to ENI spec V1.0.1, 0x100 = Compatibility to ENI spec V1.0.2)

Output Port Vendor Id:

Enter output port vendor id of the MainDevice (0 = All Vendors, 1..n = Specific Vendor)

Word-Aligned EtherCAT Datagrams:

Enable if EtherCAT datagrams should be word aligned

Cyclic Frame Layout:

Enter cyclic frame layout mode (0 = default, 1 = single logical command per frame)

Ethernet Type UDP:
../_images/ethercat-frame.png
Remove DC NOP Command:

Does not include NOP Command in ENI

Cable Redundancy:

Sets disable LRW for all SubDevices to use cable redundancy and enables an opportunity to select a second adapter and link-layer

Junction Redundancy:

Allows to user to scan also with connected junction redundancy

Local System
../_images/local.png
Display Group:

Shows or hides group

Lock Group:

Locks or unlocks group

Network Adapter:

Enter index of Network Adapter in the Network Adapter List

Show Network Adapter:

Enable if user should be able to view and change the Network Adapter

Lock Network Adapter:

Enable if user should not be able to change the Network Adapter

Remote System
../_images/ras.png
Display Group:

Shows or hides group

Lock Group:

Locks or unlocks group

Protocol:

Select protocol for Remote System

Show Protocol:

Enable if user should be able to view and change the protocol

Lock Protocol:

Enable if user should be not able to change the protocol

IP Address:

Enter IP Address for Remote System

Show IP Address:

Enable if user should be able to view and change the IP Address

Lock IP Address:

Enable if user should be not able to change the IP Address

Port:

Enter Port for Remote System

Show Port:

Enable if user should be able to view and change the Port”

Lock Port:

Enable if user should be not able to change the Port

MainDevice-Instance:

Enter MainDevice-Instance number

Show MainDevice-Instance:

Enable if user should be able to view and change the MainDevice-Instance

Lock MainDevice-Instance:

Enable if user should be not able to change the MainDevice-Instance

Secure Token:

Enter secure token (string based secure token which must be known from client and server)

Show Secure Token:

Enable if user should be able to view and change the secure token

Lock Secure Token:

Enable if user should be not able to change the secure token

TLS Data:

Enter TLS data (depending on the specific TLS mode this is e.g. the path of the certificate)

Show TLS Data:

Enable if user should be able to view and change the TLS data

Lock TLS Data:

Enable if user should be not able to change the TLS data

TLS Mode:

Enter TLS mode (0 = None, 1 = Certificate, 2 = Root Certificate)

Note

This feature requires the RAS client library with TLS/SSL support (e.g. EcMasterRasClientTls.dll), which is included in the RAS TLS/SSL feature pack and must be copied into our installation directory. It is also based on OpenSSL V3.6.0, which means that the required libaries (e.g. Win32OpenSSL-3_6_0.exe) must be installed: https://slproweb.com/products/Win32OpenSSL.html

Offline Diagnosis
../_images/capture.png
Display Group:

Shows or hides group

Lock Group:

Locks or unlocks group

Simulator Functions
Display Group:

Shows or hides group

Lock Group:

Locks or unlocks group

Distributed Clocks
../_images/master-dc.png
Display Group:

Shows or hides group

Clock Adjustment:

Enter clock adjustment value (0 = default, 1 = MainDevice Shift, 2 = Bus Shift

Lock Clock Adjustment:

Enable if user should not be able to change clock adjustment

Show Clock Adjustment:

Enable if clock adjustment should be visible

Continuous Propagation Compensation:

Enter default value of Continuous Propagation Compensation

Show Continuous Propagation Compensation:

Enable if user should be able to change value of Continuous Propagation Compensation

Sync Window Monitoring:

Enter default value of Sync Window Monitoring

Show External Mode:

Enable if user should be able to use an external sync device as reference clock

System Time 64 Bit:

Enter default value of System Time 64 Bit

Features
AoE:

Enable if MainDevice supports AoE

EoE:

Enable if MainDevice supports EoE

FoE:

Enable if MainDevice supports FoE

SoE:

Enable if MainDevice supports SoE

VoE:

Enable if MainDevice supports VoE

Export Variables:

Enable if user should be able to export variables

Show Enable Column:

Shows column for enable variables on XML export

Generate SubDevice Name with Type:

Enable if type of SubDevice should be added to SubDevice names on generating ENI file

Lock Variables:

Locks or unlocks variables for editing in diagnosis mode

Show Variable Chart:

Enable if user should be able to view the chart of a variable

Show Variable Comments:

Enable if user should be able to view and edit the comments of a variable

Allow E-Bus as HC Head:

Enable if Ebus shall be allowed as HC Head

ENI Deployment:

yes: something is done with ENI after export, no: nothing done ask: you will be ask to deploy

Deployment Mode:

0: copy to path, 1: execute batch at path

Deployment Path:

Path to copy ENI or to batch for execution

Hot Connect:

Enable if MainDevice supports hot connect

Scripts
Display Group:

Shows or hides the Scripts Tab

P1:
Scan Start Script 1:

First script executed before scanning

Scan Start Script 2:

Second script executed before scanning

Scan Stop Script 3:

First script executed after scanning

Scan Stop Script 4:

Second script executed after scanning

P2:
Diag Start Script 1:

First script executed before switch to diag

Diag Start Script 2:

Second script executed before switch to diag

Diag Stop Script 3:

First script executed before switching to config

Diag Stop Script 4:

Second script executed before switching to config

Parameters
../_images/master-advanced_2.png

User defined properties, which will be written into ENI file and can be interpreted by the application inside EC-Master.

8.3. Network Mismatch Analyzer

If you have a network mismatch in your EtherCAT network it is not so easy to find the problem. For this you have the Network Mismatch Analyzer. You find it in the network main menu. If you see here some “red” entries, means that this is the start point of your network mismatch:
../_images/network-mismatch.png

8.4. Line Crossed Analyzer

If you have connected a line to a wrong port, you can see in the Line Crossed Analyzer which SubDevice is incorrectly connected. The wron entries will be red:
../_images/line-crossed.png

8.5. Inspection Report

If you want to print or show a report about the actual session, it is possible with the inspection report. I shows a lot of different data about the network communication. It is also possible to print it.
../_images/report.png

8.6. EoE Endpoint Configuration

If you want to use EoE SubDevices with your local MainDevice, you can activate the EoE Endpoint.

Note

This feature is only available if the package “Tap-Windows” from OpenVPN is installed: http://openvpn.net/index.php/download/community-downloads.html

If this package is installed, you will see the following dialog:
../_images/eoe.png
Settings
Use EoE Endpoint:

Activate EoE Endpoint support for the selected device

Network Adapter:

List of installed network adapters (TAP)

IP Address:

IP Address of the selected network adapter

8.7. Self Test Scan

To perform a Self Test Scan, a MainDevice and a target system must be selected.

../_images/self-test-scan-selected-target-system.png

The settings for the Self Test Scan can be found in file called EcEngineerWeb.xml.

After the Self Test Scan is successful, we get the following logs from the message panel.

../_images/self-test-scan-result.png

A capture file is produce after the scan and it is saved to diagnose the results. The file is saved in the path given in the capture file settings.

8.8. Settings

Can be found inside the settings menu bar.

../_images/more-settings.png

8.8.1. Message Level

../_images/settings-message-level.png

In this tab the log level of the message panel can be changed.

Log Level Settings
Message Level:

Changes what messages are displayed on the message panel

Explanation

We can see what messages are displayed depending on the selected message level (true it is displayed, false it is not displayed)

8.8.2. Capture File

A capture file could be helpful, if a very large system is given or the system is not always available. In that case the user can connect to their system, save one or more snapshots into a capture file and analyse the created capture file later.

Another use case is, that their system from time to time some problems. In that case the user can activate the automatic mode and create the snapshots at specific intervals or based on specific MainDevice notifications.

At the moment there are the following options:
../_images/settings-capture-file.png

Filename

Base file name:

Base file name of the generated capture file name

Date:

Activate, to add the date to the generated capture file name

Time:

Activate, to add the time to the generated capture file name

Content
Process data:

Activate to add process data to the capture file (read-only)

EEPROM size:

Enter size of the EEPROM (0x86 = default, 0 = no EEPROM)

ESC Register size:

Enter size of the ESC Registers (0x400 = default, 0 = no ESC register)

CoE OD of SubDevices:
Select the SubDevices of which the CoE OD information will be captured
None:

CoE OD will be not captured

All:

CoE OD will be captured of all SubDevices

User defined:

CoE OD will be captured of the defined SubDevices by physical address (e.g. 1001-1003; 1005)

CoE OD objects:

Enter index of specific objects or all objects will be collected (e.g. 0x1018; 0x7000-0x7FFF)

SDO Info Service:

Activate to use the SDO Info Service for loading the CoE Object Dictionary instead of readying the information from the ESI file.

Automatic Mode
Interval (min):

Time to wait until next snapshot will be taken

Maximum Snapshots:

Enter count of maximum snapshots

Notifications:
Select the notifications, which will trigger a snapshot. The following notifications are availabe (for more information about notifications please refer the manual of EC-Master):
  • STATECHANGED

  • ETH_LINK_CONNECTED

  • ETH_LINK_NOT_CONNECTED

  • SLAVE_STATECHANGED

  • SLAVE_PRESENCE

  • SLAVE_INITCMD_RESPONSE_ERROR

  • STATUS_SLAVE_ERROR

  • SLAVE_UNEXPECTED_STATE

  • DC_SLV_SYNC

  • DCM_SYNC

  • FRAME_RESPONSE_ERROR (optional)

  • CYCCMD_WKC_ERROR (optional)

After the snapshot(s) is / are made in diagnosis mode they can be selected in the overview in config mode:

../_images/capture.png

After the selection switching to diagnosis mode is possible. In the toolbar will be an additional combobox to select the snapshot and switch between them:

../_images/capture_2.png

8.8.3. Project Templates

If you have a lot of SubDevices with the same configuration (e.g. PDOs, InitCmds) you can use a project template. In that case new SubDevices will be first copied from this template (if available) and then taken from the ESI cache. This behaviour is also used for the bus scan.

At the moment there are the following options:
../_images/template.png

Path: Path to the selected project template

Settings
Activate:

True, for activating this project template (necessary if you want to turn it temporary off)

Ignore Revision:

The revision will be not used as search criteriom

Normally the first match will be taken from project template. If this is wrong, you can open the context menu Select from Project Template and select another one:
../_images/template_3.png

8.9. Real-time Support

Normally on Windows you do not have real-time support, but to get DCM in sync you can install the “ECAT driver” in the following modes:

Network driver

The network driver can be used from the optimized link layers

The real-time support is normally hidden in EC-EngineerWeb. It can be activate by copying the specific link layer libraries into the installation directory of EC-EngineerWeb.

For the local system, EC-EngineerWeb will turn on DCM and use the real-time clock for generating the job task cylces. For more information about how to install the “ECAT driver” please refer the manual of EC-Master Class A DCM on Windows