3. Graphical user interface
3.1. Overview
This section gives an overview about the graphical user interface:
- The graphical user interface is divided into five parts:
- Menu/Tool/Status bar:
Shows current status or mode of the EC-Inspector and allows the user to change it.
- Project Explorer:
Shows different views of the current network configuration
- Device Editor:
Show information about the selected device, like process variables.
- Short Info:
Show short information about selected device, like name, description or vendor.
- Messages:
Shows notifications which occur e.g. when the EtherCAT Device has changed its operation state or a SubDevice has been removed from (or added to) the EtherCAT network.
3.3. Project Explorer
3.3.1. Drag and Drop
It is possible to drag and drop files here to import/open them
- Project file
Opens the configuration stored in the
ECC/ECI, only one project file can be imported at a time.- ESI files
Adds the files to the ESI-Manager, it only allows
ESI,SCIandZIPfiles, multiple files are allowed.
- The context menu of one or more selected SubDevices has the following entries:
- Enable SubDevices:
Enable disabled slaves
- Disable SubDevices:
Disabled slaves will be ignored by EC-Monitor if they could not be seen by TAP
3.3.2. Configuration Mode
There are three topology visualisation views:
- Classic View
This is a tree view with multiple levels.
- Flat View
This view shows all SubDevices in a flat list, as they are connected in the EtherCAT network.
- Topology View
This view shows a graphical tree of all SubDevices, as they are connected in the EtherCAT network.
3.3.3. Learning Mode
The EC-Inspector integrates a “Learning” mode to overcome the ENI dependency. This mode generates a runtime equivalent of the ENI file by passively sniffing and extracting the requisite network configuration information from the data traffic. This learning mode can be used either with online analysis via TAP (mode 1) as well with captured Wireshark capture-files (mode 2).
After the learning was successful, the SubDevices and variables can be renamed. Also an ENI file can be exported (e.g. for EC-Simulator). To get the best result it is necessary to set the MainDevice through each state from init to operational.
3.3.4. Diagnosis Mode
There are three topology visualisation views:
- Classic View
This is a tree view with multiple levels.
- Possible device states:
Init Bootstrap
Pre-Op
Safe-Op
Op
- Flat View
This view shows all SubDevices in a flat list, as they are connected in the EtherCAT network.
- Possible device states:
Init Bootstrap
Pre-Op
Safe-Op
Op
- Topology View
This view shows a graphical tree of all SubDevices, as they are connected in the EtherCAT network.
- Possible device states:
Init Bootstrap
Pre-Op
Safe-Op
Op- Possible port states:
Bad Cable Quality
Constricted Cable Quality
Good Cable Quality
If cable quality is constricted or bad, please check the error counters of the SubDevice (for more information about the extended diagnosis, see Extended Diagnosis).
3.4. Device Editor
- This Editor gives the user the possibility to read and write information of the selected device or SubDevice:
3.5. Short Info
- This window shows short information about selected device, like name, description or vendor:
3.6. Message Window
- Shows notifications which occur e.g. when the EtherCAT MainDevice has changed its operation state or a SubDevice has been removed from (or added to) the EtherCAT network:
There is also a SDO Message Window, where only mailbox messages are shown. For example CoE messages and FoE messages. With EC-Inspector it is also possible to save the FoE file which is transferred on the network to a specific folder.