4. Examples
4.1. CoeSdoUpload
public void CoeSdoUploadExample()
{
ushort wSlaveAddress = 1012; // slave with station address 1012
ushort wObIndex = 0x1018; // object index 0x1018
byte byObSubIndex = 1; // subindex 1 (Vendor ID, which is from type UDINT with 4 bytes)
uint dwDataLen = 4; // 4 bytes
byte[] pbyData = new byte[dwDataLen];
uint dwOutDataLen = 0;
uint dwTimeout = 5000; // timeout 5s
uint dwFlags = (uint)EMailBoxFlags.NONE; // no complete access
uint dwSlaveId = m_oEcWrapper.GetSlaveId(wSlaveAddress);
ECError eRes = m_oEcWrapper.CoeSdoUpload(dwSlaveId, wObIndex, byObSubIndex, pbyData, dwDataLen, out dwOutDataLen, dwTimeout, dwFlags);
if (eRes != ECError.EC_NOERROR)
{
LogMasterError("CoeSdoUpload failed: ", eRes);
return;
}
string szValue = CEcWrapperDotNet.ConvValueToString(DN_EC_T_DEFTYPE.ARRAY_OF_BYTE, pbyData);
LogInfo("CoeSdoUpload success: " + szValue); // 02 00 00 00
}
4.2. CoeSdoDownload
public void CoeSdoDownloadExample()
{
ushort wSlaveAddress = 1012; // slave with station address 1012
ushort wObIndex = 0x40A2; // object index 0x40A2
byte byObSubIndex = 2; // subindex 2
uint dwValue = 123; // value 123
uint dwTimeout = 5000; // timeout 5s
uint dwFlags = (uint)EMailBoxFlags.NONE; // no complete access
// convert UNSIGNED32 value to 4 bytes
byte[] pbyData = null;
ECError eRes = CEcWrapperDotNet.ConvValueToBytes(DN_EC_T_DEFTYPE.UNSIGNED32, dwValue, out pbyData);
if (eRes != ECError.EC_NOERROR)
{
LogMasterError("ConvValueToBytes failed: ", eRes);
return ;
}
uint dwSlaveId = m_oEcWrapper.GetSlaveId(wSlaveAddress);
eRes = m_oEcWrapper.CoeSdoDownload(dwSlaveId, wObIndex, byObSubIndex, pbyData, (uint)pbyData.Length, dwTimeout, dwFlags);
if (eRes != ECError.EC_NOERROR)
{
LogMasterError("CoeSdoDownload failed: ", eRes);
return;
}
LogInfo("CoeSdoDownload success");
}
4.3. ReadSlaveEEPRom
public void ReadSlaveEEPRomExample()
{
bool bFixedAddressing = true; // enable fixed addressing
ushort wSlaveAddress = 1006; // slave with station address 1006
ushort wEEPRomStartOffset = 0x0; // offset 0
uint dwReadLen = 10; // 10 bytes
byte[] pwReadData = new byte[dwReadLen];
uint dwNumOutData = 0;
uint dwTimeout = 2000; // timeout 2s
ECError eRes = m_oEcWrapper.ReadSlaveEEPRom(bFixedAddressing, wSlaveAddress, wEEPRomStartOffset, pwReadData, dwReadLen, out dwNumOutData, dwTimeout);
if (eRes != ECError.EC_NOERROR)
{
LogMasterError("ReadSlaveEEPRom failed: ", eRes);
return;
}
string szValue = CEcWrapperDotNet.ConvValueToString(DN_EC_T_DEFTYPE.ARRAY_OF_BYTE, pwReadData);
LogInfo("ReadSlaveEEPRom success: " + szValue);
}
4.4. FoeFileDownload
public void FoeFileDownloadExample()
{
ushort wSlaveAddress = 1012; // slave with station address 1012
string szFileName = "foe.txt"; // filename of file in slave
byte[] pbyData = new byte[] { 1, 2, 3, 4 }; // 4 bytes
uint dwPassword = 0; // password is 0
uint dwTimeout = 2000; // timeout 2s
uint dwSlaveId = m_oEcWrapper.GetSlaveId(wSlaveAddress);
ECError eRes = m_oEcWrapper.FoeFileDownload(dwSlaveId, szFileName, (uint)szFileName.Length, pbyData, (uint)pbyData.Length, dwPassword, dwTimeout);
if (eRes != ECError.EC_NOERROR)
{
LogMasterError("FoeFileDownload failed: ", eRes);
return;
}
LogInfo("FoeFileDownload success");
}