Introduction

1. Introduction

The .NET Wrapper provides a .NET interface to use EC-Master, EC-Monitor, EC-Simulator and RAS Client/Server.

1.1. Requirements

Microsoft .NET Framework
  • Windows (x86/x64)
    • Microsoft Windows 10 and above

    • Microsoft .NET Framework 4 Client Profile

    • Microsoft Visual C++ 2015 Runtime

  • Linux (x86/x64)
    • Mono 3.2 and above (install mono-cmplete)

Microsoft .NET Core

1.2. Architecture

.NET programming interface layer model

The architecture contains 4 basic layers:

Customer .NET application or our examples (EcMasterDemoDotNet, …)
  • Demo application, written in C#

Programming Interface (EcWrapperDotNet)
  • Provides an object oriented API written in .NET

Wrapper Library (EcWrapper)
  • Native wrapper library, which provides API for object oriented access

Native Libraries
  • EC-Master Library

  • EC-Monitor LIbrary

  • EC-Simulator Library

  • RAS Client Library