emllDwXgmac

Synopsys DesignWare® Cores XGMAC Ethernet MAC IP.

See also

User Manual

Supported OS and Arch

Linux

Architecture

ARM_64

Interrupt supported

❌

Fingerprint supported

❌

Supported SoC’s

enum EC_T_DWXGMAC_TYPE

Values:

enumerator eDwXgmac_JetsonAgxOrin

MAC on Nvidia Jetson Agx Orin

enumerator eDwXgmac_JetsonAgxThor

MAC on Nvidia Jetson Agx Thor

Supported Reference Boards

The following reference boards have been successfully tested and predefined parameter sets in EcSelectLinkLayer.cpp are available.

NVIDIA Jetson AGX Orin Dev Kit

NVIDIA Jetson AGX Thor Dev Kit