1. Getting Started - step-by-step tutorial
This manual will guide you through the following steps:
Hypervisor Hardware/Software setup
Assigning an
Intel PRO/1000network adapter for real-time use (connected with EtherCAT slaves).Scan and configure the EtherCAT network.
Bring the EtherCAT network into OPERATIONAL mode.
Hint
sudo is similar to Windows run as administrator and is valid for a single command only.
Hint
sudo -s switches the user to root (administrator), all following commands then will be executed with elevated rights.
1.1. Prerequisites
PC/IPC with at least 1 Ethernet adapter.
CPU: at least 2 cores. This guide assumes a 4 cores CPU is used.
HDD: at least 10GB. Additional 50GB in case a Windows guest shall be used.
One Ethernet adapter to be used for TCP/IP (e.g. to remotely connect to the Hypervisor). This adapter has to be connected with you company network.
One additional
Intel GigabitEthernet adapter (likeI210), as some of the shipped demo scripts are preconfigured to this type of network adapter.
Several EtherCAT slaves connected with the
Intel Gigabitnetwork adapter
Caution
You must disable Secure boot in the BIOS, otherwise the Hypervisor will not work correctly!
Caution
In this tutorial the Hypervisor will be installed onto the hard disk and all data will be overwritten. Assure required data is saved before installation!
Recommended BIOS settings (for real-time operation)
USB Legacy mode has to be disabled
Hyper-Threading shall be disabled
Power saving settings have to be disabled (C-States, Speedstep, …)