1. Introduction
This guide describes setting up a private network with 2 running Linux(UBUNTU) guest VM instances (Linux I (UBUNTU) + Linux II (UBUNTU)), a RT-Linux instance (RTOS) and the Hypervisor host (Host), each pinging the others through the RtosVnet.
This manual will guide you through the following steps:
Using virtual adapter
RtosVnetSetting up the
IPaddresses for each instance/guest.Adjust additional settings
Ping each instance/guest
Caution
This guide describe only a small aspect therefore the prerequisites are important! (See Chapter Prerequisites)
Hint
The private network addresses used in this guide are in the range of 192.168.157.XXX.
1.1. Prerequisites
PC/IPC with at least installed acontis Hypervisor.
2 configured
Linux (UBUNTU)guests. Please checkoutHypervisor-LinuxGuest-Guide.1 configured
RT-Linuxguest. Please checkoutHypervisor-Quickstart-Guideif not yet done.
already used (as default pre-configured)
IPaddresses (RtosVnet):host: 192.168.157.1
RT-Linux: 192.168.157.2