8. Add an additional Ubuntu guest [OPTIONAL]
To clone an existing VM, follow the same steps as described in the Windows Guest Guide tutorial.
As an alternative of cloning the installed Ubuntu image, it’s also possible to use the ubuntu.iso install image again – like in the previous chapters – and install vm2 freshly.
Hint
The same changes of this chapter applies accordingly for more Ubuntu guests (like vm3, vm4, etc).