3. Part B - Hypervisor Host Configuration
The following shell scripts are available on the Hypervisor Host to setup and establish a remote debug connection:
command
hv_brvnetset
creates a virtual network bridge on Hypervisor Host to forward debuggerTCP/IP/UDP
packets fromLAN1
to theRTOS-32 VM
. It is required to start this script if you need to perform remote debugging of aRTOS-32
app from another machine.command
hv_brvnetclr
deletes bridge, after theRTOS-32 VM
has been stopped.the
/hv/config/brvnetconfig.sh
file contains the configuration values for the bridge.
Hint
The configuration file /hv/config/brvnetconfig.sh
must be adjusted, at least the $IP$
address needs to fit to the environment.
Hint
See chapter “Bridge virtual and physical network” in the Hypervisor Manual for details how to configure the bridge.