5. Part D - Hypervisor Host Configuration

Adjust the guest configuration setting to prepare starting the RTOS-32 Debug Monitor:

cd /hv/guests/examples/rtos-32
gedit usr_guest_config.sh

and add the following line:

export osImage=$HV_ROOT/guests/examples/rtos-32/Monvmf.bin

Start the RTOS-32 Debug Monitor:

cd /hv/guests/examples/rtos-32
hv_guest_start -view

The output of the RTOS-32 Debug Monitor should be similar to:

 RTTarget-32 Debug Monitor 6.29 Evaluation Version
 Copyright (c) 1996,2022 On Time Informatik GmbH

 Monitor Header at: 04037A3C, Current CPL: 0
 Ethernet: RTOS32Win VNet, MAC: AA-BB-CC-DD-EE-03, IP: 172.17.10.5

Open a new terminal window (right click on desktop and select ‘Open Terminal here’ or press CRTL + ALT + T)


Configure a bridge which connects the external network (where the Development PC is located) with the virtual network (where RTOS-32 is connected to). See section Bridge virtual and physical network in the Hypervisor manual for details.

Create bridged network connection:

sudo hv_brvnetset

Output of successful bridge creation:

rtv@rtv-TEST:/hv/guests/examples/rtos-32$ sudo hv_brvnetset
[sudo] password for rtv:
load vnet bridge configuration
add enp2s0 and vnet0 to bridge vnetbr
bridge name bridge id           STP enabled interfaces
vnetbr      8000.0060c8000000   no          enp2s0
                                            vnet0
ifconfig vnetbr 172.17.10.53 netmask 255.255.0.0
ip route add default via 172.17.5.2
RTNETLINK answers: No such process

Important

Remove the bridged network connection after debugging!

sudo hv_brvnetclr

Hint

See chapter “Bridge virtual and physical network” in the Hypervisor Manual for details how to configure the bridge.