1. Step by Step Hypervisor Host and RTOS-32 Configuration with System Manager and Shell Scripts

1.1. Introduction

It is recommended to carry out the steps in the order described so that you get the remote debugging running. Steps, which are marked with <optional>, can be skipped.

Important

The steps are grouped in parts A-E over Hypervisor Host and RTOS-32. Each part depends on the previous part!

On the development PC our classic EC-Win(RTOS-32) is used. On the Hypervisor Host the steps must be done by the shell and/or supplied shell scripts.

1.2. Default values:

This tutorial assumes the following default values. Adjust it accordingly to your needs in the places of occurrence.

  • $Target_HV_IP$ = 172.17.10.53 - IP address of Hypervisor Host network adapter and the bridge.

  • $Target_IP$ = 172.17.10.5 - Remote IP address of the RTOS part.

  • \\172.17.10.53\debug - Default network share (adjust share name 'debug' at /etc/samba/smb.conf if needed)

  • enp2s0 default name of the Hypervisor Host network adapter.

1.3. Prerequisites

  • EC-Win(RTOS-32) 7.1 or newer

  • acontis Hypervisor package

  • Development PC

  • Hypervisor Host (PC/IPC)

  • Visual Studio (2005-2019) with C/C++ workload

On Development PC: Visual Studio + EC-Win(RTOS-32)

On Hypervisor Host (PC/IPC): installed acontis Hypervisor package