Windows Real-time Extension & EtherCAT-Master StackΒΆ Table of Contents 1. Introduction 1.1. Documentation 1.2. Architecture of EC-Win 2. Getting Started - step-by-step tutorial 2.1. Prerequisites 2.2. Setup the Real-time Extension Runtime 2.3. Network Controller Setup 2.4. Copy the demo application 2.5. EC-Win Architecture 3. Running the EC-Master Demo Application 3.1. Assumption 3.2. Network configuration: creating the ENI file 3.3. Run the demo application in operational mode 4. Build and run EC-Master demo using Visual Studio 4.1. Visual Studio Project settings for the acontis EtherCAT master stack 4.2. Executing the demo from within Visual Studio