3. Project structure
ENISample
ENIFiles (one for eachEBIfile)LanguagesLanugage specific files
EtherCATEtherCAT Slave Information (
ESI) FilesSrcC#EniBuilder.slnVisual Studio 2015 Solution File for the C# Sample Code
SrcC#EniBuilderDnc.slnVisual Studio 2017 Solution File for the C# Sample Code (.NET Core)
SrcCppEniBuilderForCpp.slnVisual Studio 2015 Solution File for the C++ Sample Code
ESICache.xml(generated on first run)ESI-File-Cache for faster access of
ESIfilesNOTE: If you change the ESI-File-Cache, this file must be deleted!
EniBuilder.exeC# Sample Application
EniBuilderForCpp.exeC++ Sample Application
EniBuilder.logLog File
Config*.xmlSample
EBIFiles