11. Licensing

11.1. Third party Software

EC-Engineer is using the following third party software:

  • Infragistics

11.2. EC-Engineer License

For EC-Engineer we have two license models:

  • Node Locked License

  • Floating License

11.3. Node Locked License

If you choose this license model, you need an USB dongle for every single computer. This dongle must be plugged into the computer where you want to use EC-Engineer.

../_images/dongle-one-pc.png

11.4. Floating License

If you choose this license model, you need only one USB dongle with multiple floating licenses. This dongle must be plugged into your license server and all client computers will connect to this license server.

../_images/dongle-server-pc.png

Note

This requires that the “WebAdmin” of the “Code Meter” is installed on the system. Please download and install the “Code Meter Runtime” from WIBU: https://www.wibu.com/

11.4.1. Configure License Server

Install the “Dongle-Version” of EC-Engineer on your license server, plug-in your USB dongle and open the “WebAdmin”:
../_images/wibu.png
In the “WebAdmin” navigate to “Configuration Server”, select the option “Run Network Server” and press Apply:
../_images/wibu_2.png

11.4.2. Configure Client Computer

Install the “Dongle-Version” of EC-Engineer and open the “WebAdmin”:
../_images/wibu.png
In the “WebAdmin” navigate to “Configuration Network”, press add, enter your IP address of your license server and press Apply:
../_images/wibu_3.png

Now, you should be able to start EC-Engineer.

Note

If too many clients are connected you will, you will receive the following error message:

../_images/wibu_4.png

In that case, you should try to close unused EC-Engineer instances or buy more floating licenses.

11.5. License Update

11.5.1. Request License Update

Step 1: Install the “Dongle-Version” of EC-Engineer and open the “CodeMeter Control Center”:
../_images/wibu_5.png

If the selected license is a virtual dongle, simply drag and drop the WibuCmLIF file onto the CodeMeter Control Center. Otherwise, the dongle should already be visible.

Step 2: In the “CodeMeter Control Center” open the “CmFAS Assistent” by clicking on License Update:
../_images/wibu_6.png
Step 3: Now, follow the assistant until you can select a file name:
../_images/wibu_7.png
Step 4: Select “Create license request”:
../_images/wibu_8.png
Step 5: Select “Extend existing license”:
../_images/wibu_9.png
Step 6: Keep the selected the vendor:
../_images/wibu_10.png
Step 7: Select the file name:
../_images/wibu_11.png
Step 8: Finish the assistant:
../_images/wibu_12.png

Step 9: Your license request file *.WibuCmRaC has been successfully created. Please send it to sales@acontis.com

11.5.2. Install License Update

After you have been sent your license request file you will receive the license update file *.WibuCmRaU.

Step 1: Connect your dongle.

Step 2: Copy the license update file to your desktop.

Step 3: Double-click on the license update file:
../_images/wibu_13.png

11.6. Dongle Firmware Update

Step 1: Install the “Dongle-Version” of EC-Engineer and open the “CodeMeter Control Center”:
../_images/wibu_5.png
Step 2: In the “CodeMeter Control Center” click on Update Firmware of selected Cm Dongle:
../_images/wibu_14.png
Step 3: Execute firmware update by pressing OK:
../_images/wibu_15.png
Step 4: Wait until firmware update was executed:
../_images/wibu_16.png
Step 5: Firmware update was done and dongle can be removed:
../_images/wibu_17.png

11.7. Expiration Date Dongle

If you chosed a expiration dongle you can find your expiration date in the ‘About Dialog’. If you have an unlimited dongle you will not see a date in the dialog.
../_images/about.png

If you see this date you can not use an Engineer which was released after the expiration date, but all older ones are possible.

If you try to start an Engineer which is newer than the expiration date, you will get the following error:
../_images/wibu_18.png