7. Simulator Mode

With the new EC-Engineer it is possible to use the EC-Simulator.

There are two possibilities:

  1. The user can activate the Simulator Tabs and create an EXI File to start the simulator. It is also possible to connect to a remote system with a running Simulator. More information about offline configuration and remote diagnosis can be found in the Getting Started Chapter.

  2. The second possibility is, that the user has already a configuration with a MainDevice. Now the user can do a right click on Simulation in the toolbar to start EC-Simulator with this config. Now the user has a running Simulator and running EC-Master.

../_images/architecture_2.png