6. Additional Tools

6.1. ESI-Manager

ESI-Manager can be found through the main menu File -> ESI-Manager.

This dialog helps the user to administrate his ESI and SCI files. Here, he can add/delete/export ESI and SCI files.
../_images/esi-manager.png

6.2. Network Mismatch Analyzer

If you have a network mismatch in your EtherCAT network it is not so easy to find the problem. For this you have the Network Mismatch Analyzer. You find it in the network main menu. If you see here some “red” entries, means that this is the start point of your network mismatch:
../_images/network-mismatch.png

6.3. Line Crossed Analyzer

If you have connected a line to a wrong port, you can see in the Line Crossed Analyzer which SubDevice is incorrectly connected. The wron entries will be red:
../_images/line-crossed.png

6.4. Inspection Report

If you want to print or show a report about the actual session, it is possible with the inspection report. I shows a lot of different data about the network communication. It is also possible to print a PDF.
../_images/report.png

6.5. EoE Endpoint Configuration

If you want to use EoE SubDevices with your local MainDevice, you can activate the EoE Endpoint.

Note

This feature is only available if the package “Tap-Windows” from OpenVPN is installed: http://openvpn.net/index.php/download/community-downloads.html

If this package is installed, you will see the following dialog:
../_images/eoe.png
Settings
Use EoE Endpoint:

Activate EoE Endpoint support for the selected device

Network Adapter:

List of installed network adapters (TAP)

IP Address:

IP Address of the selected network adapter

6.6. Settings

Can be found inside the settings menu bar.

../_images/more-settings.png

6.6.1. General

../_images/settings-general.png
Appearance
Language:

Changes the current language

Theme:

Changes the current theme

6.6.2. Message Level

../_images/settings-message-level.png

In this tab the log level of the message panel can be changed.

Log Level Settings
Message Level:

Changes what messages are displayed on the message panel

Explanation

We can see what messages are displayed depending on the selected message level (true it is displayed, false it is not displayed)

6.6.3. Capture File

A capture file could be helpful, if a very large system is given or the system is not always available. In that case the user can connect to their system, save one or more snapshots into a capture file and analyse the created capture file later.

Another use case is, that their system from time to time some problems. In that case the user can activate the automatic mode and create the snapshots at specific intervals or based on specific MainDevice notifications.

At the moment there are the following options:
../_images/settings-capture-file.png
Filename
Folder:

Path, where the capture files should be saved

Base file name:

Base file name of the generated capture file name

Date:

Activate, to add the date to the generated capture file name

Time:

Activate, to add the time to the generated capture file name

IP Address:

Activate, to add the IP address to the generated capture file name

Preview:

Shows a preview of the generated capture file name

Content
Process data:

Activate to add process data to the capture file (read-only)

EEPROM size:

Enter size of the EEPROM (0x86 = default, 0 = no EEPROM)

ESC Register size:

Enter size of the ESC Registers (0x400 = default, 0 = no ESC register)

CoE OD of SubDevices:
Select the SubDevices of which the CoE OD information will be captured
None:

CoE OD will be not captured

All:

CoE OD will be captured of all SubDevices

User defined:

CoE OD will be captured of the defined SubDevices by physical address (e.g. 1001-1003; 1005)

CoE OD objects:

Enter index of specific objects or all objects will be collected (e.g. 0x1018; 0x7000-0x7FFF)

SDO Info Service:

Activate to use the SDO Info Service for loading the CoE Object Dictionary instead of readying the information from the ESI file.

Automatic Mode
Interval (min):

Time to wait until next snapshot will be taken

Maximum Snapshots:

Enter count of maximum snapshots

Notifications:
Select the notifications, which will trigger a snapshot. The following notifications are availabe (for more information about notifications please refer the manual of EC-Master):
  • STATECHANGED

  • ETH_LINK_CONNECTED

  • ETH_LINK_NOT_CONNECTED

  • SLAVE_STATECHANGED

  • SLAVE_PRESENCE

  • SLAVE_INITCMD_RESPONSE_ERROR

  • STATUS_SLAVE_ERROR

  • SLAVE_UNEXPECTED_STATE

  • DC_SLV_SYNC

  • DCM_SYNC

After the snapshot(s) is / are made in diagnosis mode they can be selected in the overview in config mode:

../_images/capture.png
After the selection switching to diagnosis mode is possible. In the toolbar will be an additional combobox to select the snapshot and switch between them:
../_images/capture_2.png

6.6.4. Expert

../_images/settings-expert.png
Debug Message Levels
GUI Level

Changes the GUI debug message level

MainDevice Debug Message Level

Changes the MainDevice debug message level

Self Test Scan Settings
Detect Bad Connection

(De-)Activates bad connection detection

Frame Size Min

Changes the min frame size

Frame Size Max

Changes the max frame size

Frame Size Step

Changes the frame step size

Frame Count

Changes the frame count

Clear Error Counters

Resets the error counters on the MainDevice

Automatic Snapshots

Enables the creation of a snapshot after running a successful Self Test Scan

6.6.5. Settings File

Inside this file the user can modify all settings, including some that are not present in the settings dialog.

Warning

Only modify this file if you know what you are doing.

../_images/settings-settings-file.png

The file can be located either at “C:/ProgramData/EC-Engineer/User.<username>.xml” or insdie the install directory.

6.7. Real-time Support

Normally on Windows you do not have real-time support, but to get DCM in sync you can install the “ECAT driver” in the following modes:

Network driver

The network driver can be used from the optimized link layers

The real-time support is normally hidden in EC-Lyser. It can be activate by copying the specific link layer libraries into the installation directory of EC-Lyser.

For the local system, EC-Lyser will turn on DCM and use the real-time clock for generating the job task cylces. For more information about how to install the “ECAT driver” please refer the manual of EC-Master Class A DCM on Windows