8. Customization
8.1. Multi-Language-Support
EC-Lyser supports multiple languages, which can be changed at runtime. Adding support for further lanuages is quite easy because it is just a simple XML file which must be added to the kit.
All language files are stored in: “%ProgramFiles%/acontis_technologies/EC-Lyser/Languages/…`
EC-Lyser has also full UNICODE support, which means that it is also possible to support Asian languages:
8.2. Themes
EC-Lyser supports multiple themes, which can be changed during compile time. Adding support for further themes is quite easy because a theme consists of a couple of XAML files which must be added to the kit.
Five themes are already included into EC-Lyser:
- Royal Light Theme
- IG Theme
- Luna Theme
- Office 2010 Blue Theme
- Office 2013 Theme