2. Installation
2.1. Setup Process
The EC-Lyser can be installed by executing the setup.exe (requires administrator privileges) and follow the screen instructions:
Welcome page:
License Agreement:
Select Installation Folder:
Confirm Installation:
Installing:
Installation Complete:
2.2. Silent Installation (optional)
The EC-Lyser can be also installed in silent mode by using the command line parameters of msiexec.
Sample 1: Installs EC-Lyser into default installation folder
msiexec /i c:/temp/ECLyserSetup.msi /quiet /qn /norestart /log c:/temp/install.log
Sample 2: Installs EC-Lyser into “C:/EC-Lyser”
msiexec /i c:/temp/ECLyserSetup.msi /quiet /qn /norestart /log c:/temp/install.log INSTALLLOCATION="C:/EC-Lyser"
For more information please refer command line parameters of msiexec.
Note
The system requirements (see section “1.3”) will be not checked!
2.3. File and Folder Structure
The setup process will copy all necessary files into the following folder:
- Installation directory:
/DocRelease notes and the user manual
/EECFiles for mapping emergency error codes
/LanguagesLanugage specific files
/EC-Lyser.exe
EcWrapper.dll
…
- All users directory: ( %ALLUSERSPROFILE%/EC-Lyser, like C:/ProgramData/EC-Lyser)
/CAPTURECapture files which can be analysed in offline diagnosis mode (see Capture File)
/EMIEtherCAT MainDevice Information files
/EtherCATEtherCAT SubDevice Information (
ESI) Files. Can be modified via ESI-Manager/- ESICache.xml (ESI-File-Cache for faster access of
ESIfiles) EC-Lyser.log (Log File)
User.myusername.xml (User specific settings)
- ESICache.xml (ESI-File-Cache for faster access of
2.4. NDIS Driver
The Network Driver Interface Specification (NDIS) is the specification for a network driver architecture that allows transport protocols like TCP/IP to communicate with an underlying physical network adapter. For sending and receiving EtherCAT frames in Windows, EC-Lyser makes use of the well-known Windows packet capture library, WinPcap. However, WinPcap was based on the NDIS 5.x driver model, and development has ceased. The latest versions of Windows 10 do not support this old NDIS 5.x version anymore, so now EC-Lyser (V3.2 and higher) includes an installation package in the install directory of EC-Lyser to install the acontis NDIS 6.x Filter Module EcatNdis.sys. With this new Filter Module and the new NDIS Link Layer emllNdis.dll, it is now possible for EC-Lyser to work without WinPcap on all Windows 10 versions.
Note
Please restart EC-Lyser after the NDIS installation.