4. Graphical user interface
4.1. Overview
This section gives an overview about the graphical user interface:
- The graphical user interface is divided into five parts:
- Menu/Tool/Status bar:
Shows current status or mode of the EC-Lyser and allows the user to change it.
- Project Explorer:
Shows different views of the current network configuration
- Device Editor:
Show information about the selected device, like process variables.
- Short Info:
Show short information about selected device, like name, description or vendor.
- Messages:
Shows notifications which occur e.g. when the EtherCAT Device has changed its operation state or a SubDevice has been removed from (or added to) the EtherCAT network.
4.3. Project Explorer
4.3.1. Drag and Drop
It is possible to drag and drop files here to import/open them
- Project file
Opens the configuration stored in the
ECC/ECI, only one project file can be imported at a time.- ESI files
Adds the files to the ESI-Manager, it only allows
ESI,SCIandZIPfiles, multiple files are allowed.
4.3.2. Diagnosis Mode
There are three topology visualisation views:
- Classic View
This is a tree view with multiple levels.
- Possible device states:
Init Bootstrap
Pre-Op
Safe-Op
Op
- Flat View
This view shows all SubDevices in a flat list, as they are connected in the EtherCAT network.
- Possible device states:
Init Bootstrap
Pre-Op
Safe-Op
Op
- Topology View
This view shows a graphical tree of all SubDevices, as they are connected in the EtherCAT network.
- Possible device states:
Init Bootstrap
Pre-Op
Safe-Op
Op- Possible port states:
Bad Cable Quality
Constricted Cable Quality
Good Cable Quality
If cable quality is constricted or bad, please check the error counters of the SubDevice (for more information about the extended diagnosis, see Extended Diagnosis).
4.4. Device Editor
- This Editor gives the user the possibility to read and write information of the selected device or SubDevice:
4.5. Short Info
- This window shows short information about selected device, like name, description or vendor:
4.6. Message Window
- Shows notifications which occur e.g. when the EtherCAT MainDevice has changed its operation state or a SubDevice has been removed from (or added to) the EtherCAT network: